Enginursday: EnLightningment

In this week's Enginursday post, Joel discusses how he went about making a control box for a large scale interactive EL wire art installation.

Burning Man is right around the corner, so what better time to talk about large interactive art installations and electronics?

By now, it should come as no surprise that SparkFun is a supporter of the Burning Man festival as well as the regional burns held across the world. Our own CEO, Nathan, has given an internal Lunch & Learn on how to survive Burning Man your first year. Not to mention the numerous Burn inspired projects scattered across our site. Burners are no strangers to electronics and the DIY culture. Some of the most amazing interactive art of our time is being created for and at these festivals. For the past three years, these gatherings and the art they inspire has become a big part of my life. Since my first exposure at the Apogaea festival in 2012, I've been immersed in the art side of the festival and have enjoyed being able to contribute in a meaningful way. My fist taste of artistic gratitude came while helping my friend and fellow hackerspace member John English build SoundPuddle, a sound interactive space, which was awarded the largest art grant in Apo history at that time.

SoundPuddle

SoundPuddle making an appearance at the 2014 Denver Mini Maker Faire.

This year, Apogaea was giving away more money in art grants than any previous year. Needless to say, many people applied, much more than there was money to distribute. I, unfortunately, was one of the ones who did not receive an art grant, but that didn't mean that there wouldn't be plenty of other projects to help with. John received another grant to create a whole new sculpture, which would become Lumenexus. This was to be brought in addition to SoundPuddle. My friend and fellow hackerspace member, Liz, was also a grant recipient. Her piece was entitled EnLightningment, and it was a nine-foot-tall archway covered in EL wire made to look like lightning. The idea came from an EL wire lightning dress she had made a few years earlier. Since we had so many art pieces and so many members of our hackerspace, Solid State Depot, were going to be at the festival, we decided to create our own theme camp: Electron Village.

As the festival drew near, the amount of hours being put into each project grew exponentially. While I was simply helping with the build process on Lumenexus (mostly soldering), I was asked to help EnLightningment with a much larger task: building the control circuitry. I had never built something on such a large scale and had never tried to control that much EL wire before, but I knew it could be done. Thusly the crunch to get EnLightningment up and running began.

First, the structure had to be made and covered in the EL wire before we could design the control box. Liz and her partner for the project, Steve, set out to make the structure and map out where the EL wire would go on each panel.

building the panels

Building the panels.

El wire map

Mapping out where each color of EL wire will fit on each panel.

With the panels built and painted, the next step was to painstakingly cut, strip, solder and attach each piece of EL wire. With roughly 450 ft. of EL wire, that's a lot of work. Most EL wire used for costumes and other smaller projects is thin and could be brighter. For a project of this scale, some larger wire was needed. Thicker, brighter EL wire was purchased, as well as some beefier inverters. That said, we did end up using a few of the SparkFun 12V inverters, and they worked just as well.

EL Wire

stripping leftovers

To make the EL wire look like lightning, fishing line was use to tie kinks into sections of each EL strip. This was very time consuming, but they did a fantastic job of making it look realistic.

wiring up panel

The panels were connected together using an aerial performance rig, which would serve as the foundation for the whole piece.

connecting panels

Making good use of the hackerspace parking lot.

test build

Once each piece of EL wire was in place, it was time to get cracking on the control box. I knew that this would be too big a task for any one board, so I decided to go with a master/slave style system. For my master control board, I used a SparkFun Arduino Mega Pro 5V. I then used four EL Sequencers as my slave devices. Two DC/DC converters were used to drop the 12V coming off the battery down to 5V for all the boards. We also used some fuses to isolate sections of the circuit, as well as a few extra filtering caps on the converters. Last is the inverters mentioned above. You can (sort of) see the layout in the image below.

control circuitry

For communication, a single UART line was bussed from the Mego Pro's Tx pin to the Rx pin on each EL Sequencer. Then, two digital I/O pins on each Sequencer were hard wired to give them each a unique address. One board had both tied high, one with both tied low, and two with one high and one low. That way, we could broadcast commands to all four boards with only one transmission.

Not every AC line on each sequencer was used, and we lumped EL wire strips into groups of roughly equal lengths for each board to control so that one wouldn't be working harder than any of the others. Colored segments were given names like R1 for each of the red, blue, green, white and eggshell segments. Here's how we broke it down:

sequencer map

As for the interactivity, I decided to throw as many sensors as we had time to make on it and see what worked best in which scenarios. The final choices ended up being light, sound, and motion. The installation just sits and flickers about once every 15 seconds or so to act as an attention grabber. If you walk into the archway, a weatherproof ultrasonic sensor detects your presence and sets off a more frequent lightning storm. Once inside, the light sensor, created by sticking a photoresistor inside a long piece of painted PVC pipe with an LED key chain attached to it, and the sound sensor, a SparkFun Sound Detector board, would pick up participants' voices and light from costumes, adding to the light show. And, if a nearby sound camp started bumping some tunes, it would go into sound saturation mode and give you an amazing light show to accompany your music.

While the electronics were easy to build, coding the multi-layered levels of interaction was a little over my head. Luckily, another hackerspace member and electronics wizard, Dan Julio, helped us get the code in working order.

alt text

Dan typing away on the EnLightningment master code. If you look close, you can see a more finished version of the control board in the background.

It was finally time to put everything together and see if it worked. We used a simple storage tub to house the battery and electronics, and all the EL wire had to be fed into the tub from one side of the installation. It's hard to see in the picture below, but everything powered on and worked pretty well out of the gate.

alt text

There was some tweaking here and there, but the result was incredible from the moment we fired it up.

ReplaceMeOpen

ReplaceMeClose

It was very exciting to see it working, but we still had lots of work to do and very little time left. One of the last parts was power and how we were going to get more. I had been working on a solar panel rig and finished it up to bring to the festival in case all the batteries we brought weren't enough. Fortunately, we were able to power the whole project off of one battery for the entire six days we were there (granted it was only on from sunset to sunrise usually).

alt text

The only thing left was to add a little flair...

alt text

...and we were off.

alt text

Sometimes it's nice to have an easy-setup art installation. It took Steve and Liz about two hours to set the whole thing up, vs. several days for the other installations.

alt text

Once at the festival with all our art up and running, it was time to sit back, relax, and enjoy our creation.

ReplaceMeOpen

ReplaceMeClose

I hope you enjoyed this Enginursday post. If you have any questions or comments, please post them below. Thanks for reading.