We are selling our "older" reflow oven for the low low price of $2000 or a reasonable offer.
Update: The oven has sold! Thanks for your interest.
Here it is, your second chance to own a piece of SparkFun history. We are looking to pass along our 2nd purchased reflow oven, the Manncorp SMT 460c reflow oven.
You may remember back in early 2011 when we sold "Gramps." He was purchased by a local company called Aniomagic. Turns out, we sell some of their gear. He served us well, and was replaced by this SMT 460c reflow oven. This oven has also served us well, cooking many thousands, if not millions, of SparkFun circuit boards.
This oven is a vintage 2000, 3-zone, lead-free capable reflow oven. The 3rd zone is both top and bottom heat, while the first two are just top. It has both a standard conveyor and a pin conveyor that allows you to elevate boards off of the standard conveyor.
This pin conveyor is beneficial for double sided boards, you don't have to worry about knocking components off the underside. It is also set up with auto oilers for the chain, which is very convenient. The standard conveyor is approximately 18 inches wide, and the pin conveyor is adjustable from 18" down to almost 2". So you can cook a wide variety of shapes and sizes of boards. Overall dimensions of the oven are 13'x5'x5' (LxWxH). Power requirement is 230V/70A, 3 phase. Approximate weight of 2400lbs. This oven comes with a full user manual, data sheet, and maintenance instructions.
We're sad to see this great oven go, but it's time. We hope it finds a good home! We're asking $2000, but are willing to entertain reasonable offers. If you're interested, please email us!
You can check out the Craigslist ad here.