Learn how data.sparkfun.com can help you not just collect data, but also use that data to make hypothesizes, see trends, and make adjustments to a variety of systems.
One year ago, around this time, I began a new hobby: building and maintaining aquaponic systems. You may recall some of my previous aquaponic posts:
It has been a non-stop adventure, and everyday brings new challenges and rewards. It has also been a great opportunity to blend my love for electronics with my love for the aquatic. Aside from my two home systems, I also helped organize a group build project at my local hackerspace, Solid State Depot. The idea was to give those who had never built an aquaponic system a chance to see what the process was like. My intent was for this system to become both a teaching tool as well as adding a little decor to the hackerspace.
Over the course of three weekends, myself and many others from both the hackerspace community and the aquaponics community came to contribute to the group build. The system has been up and running since May, 2014.
Unlike my systems at home, this one did not receive my full attention. I can be absent from the space for an entire week, at times. As the peak of summer drew near, I started to notice that the water temperature fluctuated more than fish tend to like and were much higher than the optimal aquarium temperature, even for tropical fish. I knew if I didn't do something about this soon, it could jeopardize my fish's health. It was time to find an embedded solution to both monitor and control the water temperature.
About the time I discovered this problem was the same time SparkFun's free data service, data.sparkfun.com aka Phant, was launched. If you haven't checked it out yet, it's a great way to get started with data collection and manipulation. Using our Pushing Data to Data.SparkFun.com tutorial, I connected a DS18B20 temperature sensor and a waterproof DS18B20 temperature sensor to a Raspberry Pi B+.The waterproof probe was placed in the tank, and the standard DS18B20 sensor was attached to the side of the tank stand to monitor the room temperature, with both temperatures being broadcast to data.sparkfun.com via the hackerspace network.
The raw data stream can be found here, and here is the python script I used:
import os
import os.path
import glob
import time
from datetime import datetime
import httplib, urllib#http and url libs used for HTTP POSTs
import socket# socket used to get host name/IP
#################
## Phant Stuff ##
#################
server = "data.sparkfun.com" # base URL of your feed
publicKey = "yourpublickey" # public key, everyone can see this
privateKey = "yourprivatekey"# private key, only you should know
fields = ["date", "time", "temp"]#Your feed's data fields
#These lines connect to the DS18B20 Temp Sensor
os.system('modprobe w1-gpio')
os.system('modprobe w1-therm')
device_file = '/sys/bus/w1/devices/28-0000052688c3/w1_slave'#use your devices address(es)
device_file2 = '/sys/bus/w1/devices/28-000005313015/w1_slave'
###########
#Functions#
###########
def read_temp_raw(temp_choice):
if temp_choice == 0:
f = open(device_file, 'r')
else:
f = open(device_file2, 'r')
lines = f.readlines()
f.close()
return lines
def read_temp(read_choice):
if read_choice == 0:
lines = read_temp_raw(0)
else:
lines = read_temp_raw(1)
while lines[0].strip()[-3:] != 'YES':
time.sleep(0.2)
lines = read_temp_raw()
equals_pos = lines[1].find('t=')
if equals_pos != -1:
temp_string = lines[1][equals_pos+2:]
temp_c = float(temp_string) / 1000.0
temp_f = temp_c * 9.0 / 5.0 + 32.0
return "%.2f" % temp_f
def post_data():
temp0 = read_temp(0)
temp1 = read_temp(1)
print("Sending an update!")
# Our first job is to create the data set. Should turn into
# something like "light=1234&switch=0&name=raspberrypi"
data = {} # Create empty set, then fill in with our three fields:
# Field 0, light, gets the local time:
data[fields[0]] = temp0
# Field 1, switch, gets the switch status:
data[fields[1]] = temp1
# Next, we need to encode that data into a url format:
params = urllib.urlencode(data)
# Now we need to set up our headers:
headers = {} # start with an empty set
# These are static, should be there every time:
headers["Content-Type"] = "application/x-www-form-urlencoded"
headers["Connection"] = "close"
headers["Content-Length"] = len(params) # length of data
headers["Phant-Private-Key"] = privateKey # private key header
# Now we initiate a connection, and post the data
c = httplib.HTTPConnection(server)
# Here's the magic, our reqeust format is POST, we want
# to send the data to data.sparkfun.com/input/PUBLIC_KEY.txt
# and include both our data (params) and headers
c.request("POST", "/input/" + publicKey + ".txt", params, headers)
r = c.getresponse() # Get the server's response and print print r.status, r.reason
while True:
print("H2O temp = " + read_temp(0) + "F")
print("Room temp = " + read_temp(1) + "F")
post_data()
time.sleep(600)
Using the documentation found on phant.io, I was able to set up some HTML pages on my Wordpress site that would dish up some Google charts containing water and room temperatures. The data revealed very unstable temperatures, just as I had suspected.
Most tropical fish enjoy temperatures between 75-80°F, however, my tank was fluctuating from as high as 87°F to as low as 67°F.
One of the main causes of the fluctuation in water temperature was the fluctuating room temperature in the hackerspace, which can swing a lot in one day. Adding in the room temperature to the graph made that even more apparent.
Though the temperature outside was starting to cool down, the hackerspace is south-facing and retains a lot of afternoon heat. That coupled with the fact that fall was right around the corner, I knew I needed a better way to control the tank temperature and fast.
To combat the heat, I attached two computer fans on the backside of the fish tank, first with tape for testing, then affixed more permanently.
At first, I left them plugged in 24/7. However, that led to the water getting too cold at night. Leaving both the heater and the fans plugged in seemed wasteful, so I sought another solution. I remembered a fellow SparkFunion using PID controllers. After asking around and doing some research, I settled on an SCT-1000 PID from Amazon and followed this tutorial to create my own PID temperature controller. The main appeal of this particular PID was the fact that it had both a heating and a cooling relay, perfect for my situation. Each outlet was labeled accordingly, 'H' for heating and 'C' for cooling.
With the PID setup, it was time to wait and see if it would make a difference. The data told no lies. The water temperature had stabilized!
As expected, the water temp stayed within the 73-76°F no matter what the room temperature was. My solution had been found.
The tank temperature has been stable since, and the quality of life for my fish has improved. You can see the live graph here.
Now that the foundation has been laid for getting data to data.sparkfun.com and visualizing that data, finding new parameters to measure is just a few lines of code away. I'm currently working on getting my home systems up on Phant, monitoring temp and pH. From there, I hope to create an all-in-one, open-source aquarium monitoring solution, combing the time-lapse I showed in my previous posts with the data monitoring. I would also like to have the Raspberry Pi handle the PID control as well, having everything in one device. When that day comes, I'll be sure to share it with everyone who loves this hobby as much as I do. Thanks for reading!