Embedded Micro's new IDE and the Lucid language.
For me, Field Programmable Gate Arrays (FPGAs) have been the penultimate frontier of electrical engineering design (the ultimate would be fabricating our own chips, but once again, that's a topic for a different blog post). In discussing FPGAs with some of my SparkFun colleagues, we agree that they're hard to casually tinker with. You don't just "play around" with them. FPGAs are programmed in their own languages (usually Verilog or VHDL), using techniques based on synchronous hardware, and developed using software that's extremely sophisticated. Getting into them usually involves a very steep learning curve.
I've been on teams that built FPGA based designs a couple of times before, but it's not a world I've comfortably settled into -- I get pulled back into regular software design before I'm really up to speed. The FPGA design suites are big, full of menus, pages, tabs and modes, all described in unfamiliar terminology, which takes time to get to know. A lot of my experience was clicking on the wrong option, then having to figure out how to backtrack.
Justin Rajewski, the Founder and CEO of Embedded Micro, came to us earlier this year with an announcement: they were introducing a new language to ease the transition into FPGA development. I was curious to take a closer look -- could they lower the learning curve, and perhaps make it possible for a beginner to casually experiment with an FPGA?
Embedded Micro successfully Kickstarted the Mojo development board in 2013, and it's been revised a couple of times since then.
The board is currently on version 3, which has:
The XC6SLX9 FPGA is the heart of the board, and it has a bunch of goodies under the hood:
Developing code for an FPGA is actually describing how the above pieces are configured and interconnected. This could range from a set of simple binary logic operations to a very sophisticated plan for a mathematical algorithm or communication interface. If you want to take a deeper look at the FPGA itself, here is the family datasheet.
In addition to the Mojo hardware, Embedded Micro wrote a series of tutorials that guide the beginner through using the Xilinx tools to develop Verilog code. But, as mentioned above, these tools are cumbersome, and daunting for the beginner.
To ease the transition onto the FPGA world, Embedded Micro has now introduced an IDE for the Mojo, and a new FPGA programming language called Lucid.
The IDE is greatly streamlined in comparison the the Xilinx tools. It's a single window, with a multi-tab editor, and relatively few buttons and menus. One button builds the code, another loads it on to the board. Since it only supports the Mojo board, a lot of the options present in the Xilinx tools simply aren't applicable.
Behind the scenes, the Mojo IDE still requires the installation of Xilinx WebpackISE, which is a huge download, and requires navigating a license manager. However, once it's installed, you don't need to open it. The Mojo IDE invokes the command line tools in the background (much the same way that the Arduino IDE invokes the GCC compiler).
Lucid itself uses syntax that's a hybrid of Verilog and C++/Java, with curly braces to denote blocks of code, which will be familiar if you've used C++ or Java (as seen in Arduino or Processing). It also includes some higher-level conceptual blocks, such as flip-flips and state machines, which are very useful for FPGA design. Here's a snippet of Lucid that implements a configurable binary counter.
module counter #(
SIZE = 8 : SIZE > 0, // Width of the output
DIV = 0 : DIV >= 0, // number of bits to use as divisor
TOP = 0 : TOP >= 0, // max value, 0 = none
// direction to count, use "up" or "down"
DIRECTION = "up" : DIRECTION == "up" || DIRECTION == "down"
)(
input clk,
input rst,
output value[SIZE]
) {
.clk(clk), .rst(rst) {
dff ctr[SIZE+DIV];
}
const MAX_VALUE = c{TOP, DIVx{1}}; // value when maxed out
always {
value = ctr.q[SIZE+DIV-1-:SIZE]; // set the output
if (DIRECTION == "up") { // when this is an up counter
ctr.d = ctr.q + 1; // increase
if (TOP != 0 && ctr.q == MAX_VALUE) { // reached the top?
ctr.d = 0; // reset
}
} else { // down counter
ctr.d = ctr.q - 1; // decrease
if (TOP != 0 && ctr.q == 0) { // reached the bottom?
ctr.d = MAX_VALUE; // reset to top
}
}
}
}
The IDE also lets you intermix Lucid and Verilog source files, which can be useful if you've already got a Verilog module that you want to include. When you press the "Build Project" button, the IDE translates the Lucid files into Verilog, then passes them to the Xilinx Verilog tools. Those intermediate Verilog files are also saved in the build tree, in case you want to export them to use in a Verilog workflow.
I've been playing with Lucid on the Mojo for about 10 days now. It's been a slow process, but more productive than 10 days with a traditional FPGA design suite. I'm finding that with fewer menus, options and buttons, I'm a lot less likely to take a wrong turn and wind up in some mode I wasn't expecting. This has allowed me to focus on troubleshooting my code, rather than the development environment.
I was hoping to have some sort of ambitious project to share for this blog post, but it's not coming together as quickly as I was hoping. My divisibility by 3 checking hardware isn't fully functional, and I'm still a ways from building an I2S port from scratch.
Working with the tools, I've also found a couple of little issues with the language and IDE. In each instance, Embedded Micro have been quick to respond. They guided me toward better Lucid practices, and updated the IDE with missing features.
Lucid is very new -- it was released on April 13th! It's still in its infancy, and has room to grow. As such, I asked Embedded Micro for a peek at their roadmap. There are some things we can expect to see:
If you're looking to jump from Arduino into FPGA programming, the Mojo has an extra advantage. The 32U4 microcontroller (the same chip as is found on the the Pro Micro) is Arduino-compatible. You can use the Arduino IDE to program the microcontroller, and add your own code that can interact with the FPGA.
Embedded Micro have released the source code for the loader firmware. It exposes some hooks to run additional user code, which are described in their Arduino IDE Tutorial.
Knowing what I know now, if I had to start fresh, I'd probably take a different path through the materials Embedded Micro provides.
I've also spent enough time playing with Lucid to develop some debugging strategies. If you get stuck, try the following:
Serial.print() calls.