Long exposure experiments with dancers, EL Wire suits, an LED and DSLR camera.
My original goal was to wirelessly control each of my student's suits to the beat during their performance way back in 2017. Shortly after their performance, I decided to document the project with a photoshoot. Everything was going according to plan until I wanted the photographer to highlight the glow from EL Wire. It was a bit harder to capture with a camera, since EL wire is not as bright as the non-addressable LEDs that were used in previous builds. We decided to try to take a few pictures in the dark. After removing the spotlight on the kids, the photographer tweaked a few camera settings on his DSLR.
As you can see in the images below, EL wire is hard to see when there are other light sources in the room. Removing the additional light source will make it easier to see and capture the EL Wire's glow on camera.
![]() |
![]() |
| EL Wire in the Light | EL Wire in the Dark |
Briefly reviewing a few photos, we had an unintended effect during their photoshoot! The images coming from the light sources started to trail whenever the kids moved around. It was not on my mind until that moment but I thought it was cool opportunity to try a little light painting [1] with EL Wire and the wireless controller's LED.
After an hour-long photoshoot and taking several pictures, we got some pretty cool shots. We experimented with no movement, slow/fast movements, and then a combination of both. The main settings that he tweaked manually as his Canon EOS 6D stood on a tripod were:
Check out the pictures with some of their camera settings below. Note that these settings will depend on your camera's image sensor and brightness of the light source(s).
A few these were a bit difficult to capture since a majority of the pictures required the kids to hold a pose for more than a second, which is hard since they are kids. This caused them to be appear ghostly and blurry for the longer exposed shots whenever they were not supposed to move. Overall, it was not too bad for our first time trying to light paint with a photographer.
Have you tried creating a light painting using EL Wire or LEDs? If so, what do you prefer? Feel free to share your light paintings and let us know your thoughts below in the comments.
See our LED page for everything you need to know to start using these components in your project.