Keep an OpenMV Mind

Five new products to support the OpenMV H7 Camera, a FLIR Lepton Module, and a new version of the :MOVE mini buggy.

Welcome, welcome, welcome! We have a load of new products to showcase today and it all starts with five new supporting products for the popular OpenMV H7 Camera, including WiFi and LCD shields, and three unique lens and module options. One of those options includes the ability to add a FLIR Lepton module, so we are now offering the sensor on its own! Rounding out the day we also have a new version of the :MOVE mini buggy for micro:bit. Now, let's take a closer look!

Customize your OpenMV H7 Cam!

OpenMV WiFi Shield

WRL-16776
Retired

The WiFi Shield gives your OpenMV Cam the ability to connect to the Internet wirelessly. This shield features an ATWINC1500 FCC Certified WiFi module that can transmit data at up to 48 Mbps, making it perfect for streaming video from the OpenMV Camera. Your OpenMV Cam's firmware already has built-in support for controlling the WiFi Shield using the network module.


OpenMV LCD Shield

LCD-16777
Retired

The LCD Shield gives your OpenMV Camera the ability to display what it sees on-the-go while not connected to your computer. This shield features a 1.8" 128x160 16-bpp (RGB565) TFT LCD display with a controllable backlight. Your OpenMV Cam's firmware already has built-in support for controlling the LCD Shield using the LCD module.


OpenMV Global Shutter Module

SEN-16775
Retired

The Global Shutter Camera Module allows your OpenMV Cam to capture high quality grayscale images not affected by motion blur. The module features the MT9V034 Global Shutter Camera Module, capable of taking snapshot pictures on demand and able to run 80 FPS in QVGA mode, 200 FPS in QQVGA mode, and 400 FPS in QQQVGA mode.


OpenMV FLIR Lepton Adapter Module

DEV-16779
Retired

FLIR Lepton 2.5 - Thermal Imaging Module

SEN-16465
$209.95

The FLIR® Lepton® Adapter Module allows your OpenMV Camera to interface with the FLIR® Lepton® (version 1, 2 or 3) thermal imaging sensors for thermal vision applications. Combining machine vision with thermal imaging allows you to better pinpoint or identify objects you wish to to measure the temperature of with astounding accuracy.

In order to help support this module, we are now offering the FLIR Lepton 2.5 Thermal Imaging Module on its own as well. Please be aware that we currently have a limit of one module per order.


OpenMV Ultra Wide Angle Lens

SEN-16778
Retired

The OpenMV Ultra Wide Angle Lens gives your OpenMV Camera the ability to see a wider field of view (FOV). This lens can easily be screwed into your existing module and has about a 100° FOV. The standard lens that ships with your OpenMV Camera has about a 70° FOV, which is good but not ideal for security applications.


Kitronik :MOVE mini MK2 buggy kit

ROB-16787
$32.50 $27.49

The Kitronik :MOVE mini MK 2 buggy kit for the BBC micro:bit is the latest version of the ever popular :MOVE mini that provides a fun introduction to robotics. The :MOVE mini is a two-wheeled robot suitable for autonomous operation, remote control projects via a Bluetooth application, or being controlled using a second BBC micro:bit via the micro:bit's radio functionality.


That's it for this week! As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram or Facebook. We’d love to see what projects you’ve made!

Never miss a new product!