Which Arduino Do You Need?
We have a new tutorial designed to help you find the right Arduino, plus a whole bunch of new products.
Arduino is a great platform for prototyping, but sometimes it can be hard to figure out exactly which board you need. We've created a tutorial called the Arduino Buyer's Guide that will hopefully alleviate some of the confusion! And now...new products!
The CUI32 is a new version of the CREATE USB Interface, based on a 32-bit PIC. The CUI32 ships with "StickOS" installed as its default firmware - this is an full operating system (!) created by Rich Testardi with an on-board BASIC compiler, line editor, debugger, profiler, and simple file system to create new firmware programs and run them, without having to install any software on your host computer.
First we have the MIDI Shield, which gives your Arduino access to the powerful MIDI communication protocol, so you can control synthesizers, sequencers, and other musical devices. This shield is great for adding complex sound control to your Arduino!
Next is the
MIDI Breakout Board, which gives your
Arduino or any other microcontroller access to the
MIDI communication protocol. It is very similar to the shield above, but can be used more easily with other microcontrollers besides the Arduino and is not a shield.
Sharp's
GP2Y1010AU0F (try saying that fast three times) is an optical air quality sensor, designed to sense dust particles. An infrared emitting diode and a phototransistor are diagonally arranged into this device, to allow it to detect the reflected light of dust in air. It is especially effective in detecting very fine particles like cigarette smoke, and is commonly used in air purifier systems. We also carry the
mating connector housing and the
mating connector.
This is a
breakout board for the very high-intensity
Luxeon Rebel LED. The board is designed to dissipate damaging heat away from the LED to the back of the board. We have this available in several colors:
green,
red,
warm white,
cool white, and
royal blue.
While we are talking about LEDs, this is a
solderless LED holder, designed specifically for our
Rebel Luxeon LEDs. This product includes both the plastic contact carrier as well as the LED retention clip.
The
Cellular Shield for Arduino includes all the parts needed to interface your
Arduino with an
SM5100B cellular module. This allows you to easily add
SMS,
GSM/
GPRS, and
TCP/IP functionalities to your Arduino-based project. All you need to add cellular functionality to your Arduino project is a SIM card (pre-paid or straight from your phone) and an antenna!
This
PIC programmer, from
Cana Kit, is a professional USB PIC Programmer offering ZIF (Zero Insertion Force) sockets, an ICSP header, and an ICD2 port for easy PIC programming. This PIC Programmer uses a USB port for power and connection to the computer, as opposed to the traditional serial port, eliminating the need for a separate power supply.
Also from
Cana Kit is the
L298 Dual H-Bridge Motor Driver Integrated Circuit. The circuit will allow you to easily and independently control two motors of up to 2A each in both directions, making it ideal for robotic applications and well suited for connection to a microcontroller requiring just a couple of control lines per motor.
Continuing with the
Cana Kit, this
USB Relay Controller/Data Acquisition Module allows computer controlled switching of external devices as well as full bi-directional communication with the external world (ideal for Data Acquisition applications) using the USB port of your computer. The controller is very flexible and can be used in many custom applications.
If you want to control the speed of a
DC motor but don't want to sacrifice any torque, this
Motor Controller from
Cana Kit is for you. This controller uses pulse-width modulation (PWM) and can provide up to a maximum continuous current of 50A to your DC motor or other DC load.
This is a nice and simple
breakout board for USB microB. This board breaks out a micro-B USB connector's VCC, GND, D- and D+ pins to a 0.1" pitch header. If you want to use the handy USB micro interface but don't want to solder tiny connections, this is for you.