Hurry! It’s Time for a Flash Sale

Now through Sunday, Dec 5, we're offering 100 promo code uses to take $40 off our SparkFun GPS-RTK2 Board - ZED-F9P (Qwiic).

If you’re trying to locate your next holiday deal, look no further!

Until Sunday, Dec 5 at 11:59 p.m. MST, the first 100 people to use promo code FLASHSALE2 will receive $40 off our SparkFun GPS-RTK2 Board - ZED-F9P (Qwiic). Simply add the board to your cart and use promo code: FLASHSALE2 at checkout. Rules and information below.

 

Flash Sale extended

Sale now extended through Sunday, Dec 5 at 11:59 p.m. MST

 

About the SparkFun GPS-RTK2 Board - ZED-F9P (Qwiic)

The SparkFun GPS-RTK2 raises the bar for high-precision GPS and is the latest in a line of powerful RTK boards featuring the ZED-F9P module from u-blox. The ZED-F9P is a top-of-the-line module for high accuracy GNSS and GPS location solutions including RTK that is capable of 10mm, three-dimensional accuracy. With this board, you will be able to know where your (or any object's) X, Y, and Z location is within roughly the width of your fingernail! The ZED-F9P is unique in that it is capable of both rover and base station operations. Utilizing our handy Qwiic system, no soldering is required to connect it to the rest of your system. However, we still have broken out 0.1"-spaced pins in case you prefer to use a breadboard.

Rules & Information for Flash Sale:

  • Add the SparkFun GPS-RTK2 Board - ZED-F9P (Qwiic) to your cart!
  • Use code "FLASHSALE2" during checkout to receive $40 off the board. There are 100 promo code uses available and a promo code use limit of one per customer.
  • Promo code will be available for use through Sunday, Dec 5 at 11:59 p.m. MST OR until all promo code uses are taken, OR stock is unavailable.
  • No rainchecks or backorders will be allowed.
  • We will not be allowing the combining of orders during this sale.
  • Distributor and reseller accounts will not be eligible.

Please note: We will be working hard to ship as many orders as quickly as possible, but we cannot guarantee same-day shipping for sale orders. Please allow additional days for sale orders to ship due to increased volume.


Want a heads up on our next holiday surprise?

Sign up for our "Deals" List for the inside scoop!