Air Quality is the Best Policy

The new ENS160 Air Quality Sensor is now available with two new SparkX boards!

Hello and welcome back to another Friday Product Post here at SparkFun Electronics! This week, we have a handful of new products to show off and it all starts with the new ENS160 Indoor Air Quality Sensor! This Qwiic-enabled breakout consists of four independent heaters and gas sensor elements based on metal oxide (MOX) technology and a controller. Following that, we have two new products from SparkX, a GNSS Antenna Splitter and a Qwiic Micro Dynamic NFC/RFID Tag. Let's jump in and take a closer look at this week's new products!

That's some nice air quality!

SparkFun Indoor Air Quality Sensor - ENS160 (Qwiic)

SEN-20844
$24.95

The SparkFun ENS160 Indoor Air Quality Sensor is a digital multi-gas sensor solution with four sensor elements that can be used in a wide range of applications including building automation, smart home, and HVAC. The independent hotplate control allows the detection of volatile organic compounds (VOCs) including ethanol, toluene, hydrogen, and oxidizing gases with superior sensitivity. The ENS160 supports intelligent algorithms to process raw sensor measurements on-chip. These algorithms calculate CO2-equivalents, TVOC, air quality indices (AQIs), and perform humidity and temperature compensation, as well as baseline management, all on-chip. Raw sensor measurements can be read for further customization.


GNSS Antenna Splitter (Power Divider) with DC Pass

SPX-21223
Retired

Our GNSS Splitter (Power Divider) lets you connect a single GNSS antenna to two boards or modules. It splits (divides) the antenna signal from Port S equally between Port 1 and Port 2. It is the perfect accessory for our NEO-D9S correction data receiver, allowing you to feed both the NEO-D9S and a separate GNSS module from a single antenna.


Qwiic Micro Dynamic NFC/RFID Tag

SPX-20691
$9.95

The STMicroelectronics ST25DV dynamic Near Frequency Communication / Radio Frequency Identification tag ICs are awesome! The Qwiic Micro Dynamic NFC/RFID Tag offers 64-kBit (8-kBytes) of EEPROM memory which can be accessed over both I2C and RF (NFC)! It's a state-of-the-art tag which conforms to ISO/IEC 15693 or NFC Forum Type 5 recommendations. You can read and write the tag's memory using NFC even while the tag is powered down or disconnected!


SparkFun Constellation MicroMod Kit

KIT-21224
Retired

The SparkFun Constellation MicroMod Kit is our newest limited edition offering that joins the ranks of the SkeleBoard and the SnowBoard. Instead of releasing a single board this year, we have opted to release a full kit, instead! This kit combines both MicroMod and Qwiic in a single box with a limited edition MicroMod ATP Carrier Board and MultiStar (this year's April Fool's Day joke). No, we aren't joking this time! Due to popular demand, we have reworked the MultiStar into a working (and much safer) celestial version of the MultiPort. Also included in this kit is a MicroMod Screw Driver and two Qwiic Cables to get you hooked up! The ATP Carrier Board and MultiStar included in this kit feature a matte black PCB with a star scape design in white silk.

Get one of these three MicroMod Processor Boards FOR FREE
with a puchase of the MicroMod Constellation Kit

How to redeem your choice of MicroMod Processor Board:

  1. Add the SparkFun Constellation MicroMod Kit to your cart!
  2. Add one of three of the following MicroMod Processors to your cart:

Additional rules: Only one free Processor per order. There is an order limit of five max per customer. No rainchecks or backorders will be allowed. We will not be allowing the combining of orders during this sale. Distributor and Reseller accounts will not be eligible.

That's it for this week. As always, we can't wait to see what you make. Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there, be kind to one another, and we'll see you next week with even more new products!

Never miss a new product!