The New RPi Camera Module 3

Raspberry Pi has released its newest iteration of the Camera Module.

Raspberry Pi is at it again! Their new Raspberry Pi Camera Module 3 is now available here at SparkFun Electronics! We have three new product that all revolve around this new version of the Pi Camera Module and we are extremely excited to share them with you. Sit a spell and take a look!

Raspberry Pi Camera Module 3

SEN-21331
$32.95

The Raspberry Pi Camera Module 3 is the latest entry in the mainstream RPi camera line-up, and the successor to the popular Camera Module 2. Built around a 12-megapixel Sony IMX708 image sensor module, Camera Module 3 offers a few key enhancements over its predecessor. Improved low-light sensitivity makes for better photos and output in situations where there's not a lot of light. The module also features powered autofocus making it easier to get a sharp picture output. Finally the Camera Module 3 features High Dynamic Range (HDR) support expanding the range of color and contrast in the output.

This product is now available for pre-order.


Raspberry Pi Camera Module 3 - Wide Angle

SEN-21332
$45.05

The Raspberry Pi Camera Module 3 is the latest entry in the mainstream RPi camera line-up, and the successor to the popular Camera Module 2. This version is still built around a 12-megapixel Sony IMX708 image sensor module (as above) but this model also features a wide-angle lens (120° field of view). It also comes in a standard lens (76° field of view) variation which is available in the related products below.

This product is now available for pre-order.


Raspberry Pi High Quality Camera M12 Mount

SEN-21333
$63.75

The Raspberry Pi High Quality Camera M12 Mount is the same high quality camera as the previous model. Many industrial users prefer to use M12-mount lenses. Previously you would have to connect them to the C-mount metalwork on the HQ Camera via an adapter. This module takes the High-Quality Camera and adds modified metalwork that supports M12-mount lenses natively.


And that's it! As always, we are supremely proud to offer these Raspberry Pi products on our site and hope that they grant all of your future Raspberry Pi projects that need imaging capabilities with the same reliability as every other Pi product. As always, we can't wait to see what you make. Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Have a great rest of your Monday and we hope you enjoy these new Raspberry Pi Products!