SparkFun gets a lift on a low-atmosphere student satellite. And we have some new products too.
CU has successfully delivered their
High Altitude Student Platform payload!
![]()

The
CU payload consists of a group of CCD cameras to collect images of celestial bodies and light intensities during the 122,500ft assent into the
stratosphere. Best of luck to the CU students working on the project! We hope to hear more about the launch scheduled for later this week.
Be sure to checkout the
live camera from within the hanger,
GPS tracking, and the
controllable camera on the hanger!

Olimex is releasing some new, very complex development boards. This board based on the
LPC2478 has the power to run Linux!

If you don't need the display, this
development board for the LPC2468 is equally as powerful!

Speaking of powerful ARM boards, this is a
LPC2378 based board with TFT color LCD and touch screen.

The powerful
GSM development board is now available in a PIC flavor. Control almost anything wherever there is cellular reception!

Another nicely packaged LCD, this is a
PIC development board with monochrome LCD and 5-way joystick.

New
AT90USB162 from Atmel is a low-cost and handy USB IC. It's like the ATmega16, with a USB bootloader!

Olimex also has a new
RFID reader. This USB-enabled device shows up as HID or CDC and reads standard 125kHz RFIDs.

This is a handy SAM7 based board that incorporates our favorite nRF24L01 2.4GHz radio. Use this as a powerful
ARM based, USB wireless widget.

That is a huge hunk of epoxy, around four LED dies. These
10mm LEDs use 4 LEDs in one package to get really bright lighting effects! Available in
Red,
Green, and
Blue.

And some photo updates. This is a nifty, low power
PIC 18F8490 dev board with LCD.

The classic
terminal board with the LPC2138 has a new pic.

The
AMOLEDs from 4DSystems have a new look as well. Lots of new features jammed into these impressive displays.