New LilyPad kits, sensors, perf boards, a crazy package tracker, and various pictures updates. Oh, and Production is moving.
  
Along with the new space, the Production department is moving down stairs. Before the move, we decided to take some quick photos for historical record. We figured you might want a peek.
12 people work very hard every day building SparkFun widgets. Their speed and quality continues to amaze me. 
We finally broke down and bought a reflow oven two years ago, shown on the left. Up until then, we were using our 
hot-plate technique. You can see our raw part stock on the right.

There's the 
pick and place machine (I'd rather call it '
chef') shown in the middle, test stations on left, stenciling area on right.  The small purple dots on the ceiling are actually the left over stars from the middle of the 
LilyPad panels:

Chef making LilyPad Accelerometers. The boards are thinner than normal (0.8mm) and the center left-over bits are rather sharp at the points making them ideal throwing stars. Suddenly, we started seeing LilyPad throwing stars all over the office.
Enough of that fun, here's the new goodies:
mini-Bully is a simple, small, and powerful board developed by the folks at Mississippi State University. It's based on the PIC24 series and uses a serial bootloader so that no external programmer is needed, only a serial connection that mates with our 
FTDI Basic Breakout. Kinda like an 
Arduino Pro Mini with a bit more fire power (40MIPS!).

This has been a dream of mine since college. I always wanted to know what really happens to a package when it gets shipped by FedEx, UPS, or USPS. How well is it taken care of? Does it really fly all the way to Memphis, Tennesse just to get re-routed to Washington state? Does my poor package get cold? Wet? How high does it go? How low does the air pressure drop? Does it get dropped? Kicked down the hall? How hard does it get shaken? All these questions can be answered with the 
Package Tracker. It's a board that has an array of sensors and the ability to log them all. Use the Package Tracker to audit the next time you ship a large, expensive piece of equipment - or when you want to verify that your shipment of DNA samples did not get too warm.

We think we have the last remaining 
XBee module listed. This unit is the high-power version (Pro), of the new line (series 2.5) with a wire antenna (!). These modules from Digi make wireless communication easy with a serial AT command set and the ability to setup simple mesh networks.

We found a good supplier of low-cost 
BAC (blood alcohol content) gas sensors. Please experiment responsibly. 

We're putting together a couple LilyPad kits for Maker Faire Austin. The 
LilyPad E-Sewing Kit is a great way to get started with wearable and textile electronics. Just a couple buttons, LEDs, and some thread and you'll have your shirt or pants wired for light. Blinky is good.

Pete's going crazy with the 3-D prototyping. Checkout what you can do with the new 
penta, hex, and 
triangle shaped perf boards. We've got enough different proto boards that we decided to create a '
Board' new category under Prototyping.

Inside the new Board category, you will find some new SMD prototyping boards as well. These 
0.5mm and 
0.65mm TQFP boards all you to breakout many of the popular processor and controllers.

New 
fingerprint scanner now available! This is a lower-cost version where you slide your finger across the sensing element. Works great, comes with easy to use software, and has a simple serial interface for uniquely identifying users.

New 
membrane keypad. This was originally designed as a custom keypad for a VOIP phone development kit. Now we get to use it for our own liking. Sealed, with an adhesive backing makes this keypad able to withstand the outside world.

What's a 
Pogo Pin? It's a very small pin that has a spring loaded head. Commonly used in test fixtures, the board under test can be quickly compressed against a 'bed of nails' test jig, run through a battery of tests, then removed without the need for soldering. We use them in our own test jigs but we figured you would have some good uses for them as well.

We now stock a 
CR2045 battery holder that is tall enough to contain our 
Lithium Ion rechargeable coin cells. Cheap, and easy to solder!

This is a 
pre-amp board that allows you to connect various low level audio devices  like guitar pickups, electret mics, and piezo discs - and connect them to larger amplifiers and audio equipment. A simple design, but a much needed glue to piece audio equipment systems together. 
And to make this perhaps the longest News post ever, we have image updates!

The 
LIS302DL breakout is finally updated with the correct breakout pins. This is a wonderfully simple low-cost 8-bit triple axis accelerometer that you will start to see in many consumer electronics.

Slight update on the 
Logomatic v2. We broke out some additional pins, improved the routing, and rotated the battery connector to be side-entry to easier connecting. If you need a flexible data logger, this is the product to checkout!

The 
LilyPad USB Link is now is sexy red, with the addition of TX and RX LEDs.