BASE Jumping with Accelerometers
A great project from a mad customer and new products in RFID, GPS, and a new WiFi module!

Well, that's one way to get back down the mountain.
Michael Cooper sent us these amazing photos and data plots:
"I thought you guys might get a kick out of this. I wrote my own
firmware for the
WiTilt, which gives 250 Hz of accelerometer data with
16x oversampling. The data is sent via Bluetooth
? connection to my Palm Tungsten,
which takes care of logging."
Jump Plot"A couple of weeks ago, I took it for a
BASE jump from my favourite
1200-foot cliff. I?ve attached data from the freefall portion of the
jump and the first few seconds of canopy flight. The grid is 1 second
on the x-axis, and 1 G on the y-axis. The black line shows total
acceleration, while the coloured lines show each axis (after
calibration). In the 'jump' plot, you can see clearly where I jump, at
the 1 second mark, and where the canopy opens, at the 9.75 second mark,
after 8.75 seconds of freefall. You can also see the point, at about 3
seconds, where wind resistance becomes significant, after which I
appear to be resting on my belly on a cushion of air."
Whooooooooooaaaaaa! That's awesome!
Canopy Plot"Opening shocks,
visibly mostly in the 'canopy' plot, are a bit of a jumble of actual
opening shock (which is quite a blow), and oscillations which show me
being kicked out under the open parachute... I've often compared the opening of a BASE parachute to a car wreck. Of
course, we like our parachutes to open fast, but I will often feel symptoms
of whiplash after a weekend of jumping.
"
Thank you so much Michael! Those pictures send chills down my spine. Keep jumping, and stay safe!
Now for slightly less adrenaline pumping photos - new products!

New
USB eval board for our
RFID readers. This simple board allows you to plug in the RFID module of your choice. Bring a card near the reader and you'll get a serial stream containing the unique ID of the card. Nice and simple. We've also posted the Eagle files to help out the SparkFun interweb of users.

GS406 is a powerful GPS receiver with a Sarantel Helical Antenna and a uBlox 4HZ engine. Now you can get solid GPS coordinates 4 times a second!

We brought back our
WiFi category just for this new module. The
WiFly is right up our alley: It's a simple to use, small, low-cost module, and this time it's for WiFi wireless. Now you can connect your embedded project over 802.11b with just a serial connection.

We've updated the pictures for our
Button Pad breakout. We've also posted the Eagle files for this board!

Yay! The way
KinetaMap was supposed to look - now with a label!