Arduino Day (Sale) Is Coming Soon
Deals so good you'll think we're joking, but we're not.
Happy Monday! Arduino Day is Saturday, April 2, but SparkFun's largest sale of the year this side of Cyber Monday starts this Friday, April 1st (it's not a trick). As is tradition, we'll have deep discounts on several Arduino products. As an added bonus to celebrate how important Arduino has been to SparkFun's very existence, we're also offering 10 percent off all SparkFun Originals for the duration of the sale. Check out all the eligible products under the "SparkFun Originals" tab at the top left of the homepage. Also take a look below for the rules of the sale. Thanks for stopping in, and we'll see you Friday for the deals!
Arduino Day Sales Rules
All sales prices will run from 12:01 a.m. MDT on Friday, April 1st, to midnight MDT on Sunday, April 3rd. Sale prices are good only while supplies last, so get in early to get the best Arduino items available. No backorders on sales items are allowed, and distributor and educator accounts will not be eligible for Arduino Day sales prices. Some items will have maximum quantities available per order.
** $6.95 $19.95 $6.95 $19.95 **
DEV-11113
SparkFun's minimal design approach to Arduino. This is a 5V Arduino running the 16MHz bootloader.
DEV-11114
SparkFun's minimal design approach to Arduino. This is a 3.3V Arduino running the 8MHz bootloader.
DEV-11021
This is the new Arduino Uno R3. In addition to all the features of the previous board, the Uno now uses an ATmega16U2 instead…
DEV-11224
This is the new Arduino Uno R3. In addition to all the features of the previous board, the Uno now uses an ATmega16U2 instead…
$12.95 $24.95 $9.95 $9.95
DEV-10914
It's blue! It's skinny! It's the Arduino Pro! SparkFun's minimal design approach to Arduino. This is a 3.3V Arduino running t…
DEV-10915
It's blue! It's skinny! It's the Arduino Pro! SparkFun's minimal design approach to Arduino. This is a 5V Arduino running the…
Retired
DEV-12757
At SparkFun we use many Arduinos and we're always looking for the simplest, most stable one. Each board is a bit different an…
Retired
DEV-12923
The MicroView is the first chip-sized Arduino compatible module that lets you see what your Arduino is thinking using a built…
Retired
$14.95 $17.95
DEV-13664
If you’re ready to step your Arduino game up from older 8-bit/16MHz microcontrollers, the SparkFun SAMD21 Mini Breakout is …
DEV-13672
If you’re ready to step your Arduino game up from older 8-bit/16MHz microcontrollers, the SparkFun SAMD21 Dev Breakout is a…
Retired