Almost Free Day Is Coming!!!
Save the date: 7/20/2016!
No, you didn't read that wrong. The single most epic day in SparkFun's history is making its comeback. If you're familiar with SparkFun lore, Free Day involved giving away a whole bunch of SparkFun gift cards to customers. Our best-documented Free Days began in 2010 and continued through 2011 and 2012. Through all of this we learned a lot about ourselves as a company and how passionate people are about free stuff. Check out the comments from past blog posts if you want some solid entertainment. After 2012 we discontinued the annual tradition for a number of reasons, but it's time to give it another go with a different twist!
What is Almost Free Day?
This year we're selling 3,000 items for $0.01 each, thus the "almost" part of Almost Free Day. We've done this for various reasons, but mostly to keep it legal. We'll have 300 each of nine different board types and one mini LilyPad bundle (SKUs 10867, 11364, 10730, 10044). None of these boards have export restrictions, so customers around the world can participate. Here are the products:
DEV-13712
The SparkFun OpenLog can store, or "log", huge amounts of serial data and act as a black box of sorts.
ROB-12859
The Big Easy Driver, designed by [Brian Schmalz](http://www.schmalzhaus.com/), is a stepper motor driver board for bi-polar s…
DEV-12660
The SparkFun MP3 Player Shield is an awesome MP3 decoder with the capabilities of storing music files onto a run-of-the-mill …
DEV-12049
LilyPad is a wearable e-textile technology designed to have large connecting pads to allow them to be sewn into clothing & co…
DEV-10867
This is 30 feet of conductive thread spun from stainless steel fiber and wound on a plastic bobbin. Use it to sew up all of y…
LCD-13003
The SparkFun Micro OLED Breakout Board breaks out a small monochrome, blue-on-black OLED. It’s "micro", but it still packs …
DEV-11364
Add a touch of magic to your wearable projects without writing a single line of code! The LilyTwinkle is a ready-to-use LilyP…
COM-13795
The SparkFun LED Array is a set of 56 red LEDs arranged in a nice 8x7 grid. This little board requires eight pins while the l…
Retired
DEV-10730
If you're looking for a simple way to add a battery to your LilyPad project, the LilyPad Coin Cell Battery Holder might do th…
Retired
DEV-12081
The Weather Shield is an easy to use Arduino shield that grants you access to barometric pressure, relative humidity, luminos…
Retired
DEV-12757
At SparkFun we use many Arduinos and we're always looking for the simplest, most stable one. Each board is a bit different an…
Retired
DEV-13741
In 2015 we developed the BadgerStick as a fun and interactive way for people to learn about soldering and engage with SparkFu…
Retired
DEV-10044
Here is a simple 5 pack of red LEDs for LilyPad, or whatever else you can dream up. Light up the night!
LilyPad is a we…
Retired
What's the catch?
These 10 different products will all be represented as one SKU. That means you won't know which product you get until it arrives. On Almost Free Day you'll just add the "Almost Free" SKU to your cart, and if you make it through checkout before the boards run out, you'll get one of the 3,000 boards.
Is there anything else?
Yes! We'll be offering some special bundles for this day only, as well as having a big sale on the SIK. If you want to get involved in Internet of Things (IoT) or wearables/e-sewing, this is a perfect opportunity with a big discount. The following three bundle options will be $74.99 on Almost Free Day and available on the front page with the one-cent SKU:
IoT Bundle -- Our Most Popular IoT boards at their lowest prices:
DEV-13321
The SparkFun Photon RedBoard, to put it simply, is a WiFi/Microcontroller development board in the Arduino form-factor for th…
Retired
WRL-13632
The SparkFun Simblee BLE Breakout board is a programmable board that allows you to add mobile app functionality via Bluetooth…
Retired
WRL-13794
The SparkFun Blynk Board is specially designed to work with the ‘widgets’ within the Blynk mobile app to create your next…
Retired
Wearables Bundle -- A great place to start with e-sewing:*
DEV-10867
This is 30 feet of conductive thread spun from stainless steel fiber and wound on a plastic bobbin. Use it to sew up all of y…
DEV-10899
Add flashy functionality to your wearable projects without writing a single line of code! The LilyTiny is a ready-to-use Lily…
DEV-11364
Add a touch of magic to your wearable projects without writing a single line of code! The LilyTwinkle is a ready-to-use LilyP…
DEV-10275
This is the LilyPad revision of our [FTDI Basic](http://www.sparkfun.com/products/9716). It is the same as our other FTDI Bas…
Retired
DEV-10274
This is the LilyPad Arduino Simple Board. It's controlled by an ATmega328 with the Arduino bootloader. It has fewer pins than…
Retired
DEV-11285
Sure, your flashing, chip-tune playing t-shirt is really cool at the party... but at some point you need to turn it off. And …
Retired
DEV-13633
The LilyPad Simblee BLE Board is a wearable development board that allows you to add mobile application functionality via Blu…
Retired
*(Bundle includes two each of 11285, 10899, and 11364)
Classic SIK -- You know it, you love it, at its lowest price yet:
KIT-12060
**As you may have seen from [our blog post](https://www.sparkfun.com/news/2241), we recently moved our injection mold for SIK…
Retired
When is Almost Free Day?
The one-cent SKU will go live at 10 a.m. MT on 7/20/2016. The above bundles will go live at the same time. The event will last as long as it takes to sell through the 3,000 boards.
What about shipping?
Unfortunately, yes, you will have to pay for shipping, but we've done a few things to help. All domestic orders over $75 will ship free, as usual. If you'd like free shipping, just add enough to your cart before Almost Free Day to hit that $75 threshold. Then, on Almost Free Day, just add the one-cent board and go! If you can't think of $75 worth of stuff you'd like, try one of the one-time-only bundles above.
What should I do before Almost Free Day?
- If you don't have a customer account, create one before 7/20/2016
- Have your payment information and shipping information ready to get through checkout fast
- Be signed in to your account before 10 a.m. MT on 7/20/2016
- Have your cart filled with everything you want (except the one-cent board or bundle) prior to 10 a.m. on 7/20/2016
- Decide if you want to buy a bundle and be ready to add it to your cart when it goes live
- Plan on potential server crashes
- Almost Free Day may result in shipping times taking longer than usual
What are the rules and restrictions?
- Customer accounts only -- no guests, educators or distributors
- Only available for online orders
- Sale prices applicable while supplies last
- No backorders allowed
- All sale prices expire at 11:59 p.m. MT on 7/20/2016
- Only one "Almost Free" SKU, one IoT Bundle and one Wearables Bundle allowed per order
- Multiple orders on a single account are allowed throughout the day
Thanks for reading. We're excited to participate in another day of madness with you!