Friday Product Post: Going Turbo!

We have another new RedBoard today and it's gone turbo-tastic! But we can't forget about the Qwiic MP3 Trigger and Lumini 8x8 Matrix, too!

Welcome back, everyone! We have another big week of new products, starting with the RedBoard Turbo. We also have the Qwiic MP3 Trigger, which just graduated up from SparkX, as well as another board to join the LuMini line (this one is an 8x8 LED matrix!). We round out the day with a smart machine vision camera from JeVois.

We felt a little nostalgic this week with our presentation!

SparkFun RedBoard Turbo - SAMD21 Development Board

DEV-14812
$22.50 $11.95

If you’re ready to step up your Arduino game from older 8-bit/16MHz microcontrollers, the SparkFun RedBoard Turbo is a formidable alternative. At its heart, the RedBoard Turbo uses the ATSAMD21G18, which is an ARM Cortex M0+, 32-bit microcontroller that can run at up to 48MHz. With an impressive 4MB of external flash memory and a UF2 (USB Flashing Format) bootloader, the RedBoard Turbo provides you with an economical and easy to use development platform with more power than the classic RedBoard.


SparkFun Qwiic MP3 Trigger

DEV-15165
Retired

Sometimes you just to play an MP3, whether it's a theme song as you enter the room or a power song when you're working out. The SparkFun Qwiic MP3 Trigger takes care of all the necessary requirements – all you need to do is send a simple I2C command and listen to whatever is on your micro SD card. Utilizing our handy Qwiic system, no soldering is required to connect it to the rest of your system. However, we still have broken out 0.1"-spaced pins in case you prefer to use a breadboard.


SparkFun LuMini LED Matrix - 8x8 (64 x APA102-2020)

COM-15047
Retired

This is the 8x8 SparkFun LuMini LED Matrix, packed with 64 individually addressable LEDs, each capable of producing 16 million colors. It provides you with a great way to add a square of light to just about anything, or even make a screen of a custom shape! LuMini is a miniaturized version of our Lumenati LED line, but instead of utilizing 5mm by 5mm APA102 LEDs (APA102-5050), LuMini uses a 2mm by 2mm package (APA102-2020). This allows for incredibly tight pixel densities, and thus, a screen with less pixelation!


JeVois Smart Machine Vision Camera

SEN-15137
Retired

The JeVois Camera is a low cost, all-in-one 1.3MP machine vision camera. With an on-board quad core CPU and MicroSD slot, all computer vision algorithms run on the device itself, and it can interface to computers or other devices, such as Arduinos, via USB or serial connection. At just 1.7 cubic inches and 17g, this sensor is one of the smallest TensorFlow-enabled, deep learning AI, smart cameras on the market today. With the added ability to run most popular machine vision frameworks (Open CV 4.0.0, Caffe, Darknet), you will have plenty of options when it comes to deciding how you want to operate your new camera!


And that's it for this week! Let us know if you liked the video format or whether you prefer the broken up videos instead. As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram or Facebook. We’d love to see what projects you’ve made!

We'll be back next week with even more fantastic new products!