This is the first part of building a keycode-based anti-theft system for a car.
If you are like me, you enjoy the charm of driving an older vehicle. The mechanical feedback from the car is more organic. You aren’t surrounded by safety and driver aid systems that jump at the opportunity to correct your oh-so human actions. These cars were born in an era when manufacturers strove to have their own look. Shoot, you still get to plug the key into the ignition! You get the point, but as much as the above is appealing, there are many shortcomings in older vehicles, one of the primary being security.
Nowadays, most cars come with keyless ignition systems as standard equipment. This technology has been used in the industry since the late nineties in high-end automobiles, and only in the last decade or so has this system made its way to the masses. These systems can certainly come with their own set of headaches, but they do make auto theft much more difficult when using less tech-savvy methods.
My goal here is to create a keycode-based security system for starting my 80’s-era soon-to-be daily driver.
Disclaimer: the motor for said daily driver is still not actually in the car, so installation of this system will be covered in a future post. This system is designed to function with a starter circuit found in a 1980’s-era Volvo.
The primary motivations behind installing this system are to disable the ability to start the vehicle without entering the proper keycode, and to make the act of “hot-wiring” the vehicle much more difficult. The intention is to be as non-invasive as possible, so this system does not require the removal of any OEM parts included in my vehicle’s starting circuit.
The photo below illustrates the concept. Lets walk through it and talk about some reasoning.
In this basic implementation I am using the car battery to supply power to my microcontroller. In this case I’m opting to use the Sparkfun Thing Plus – ESP32 WROOM . I chose this board because of its potential – most basic microcontroller boards could perform the task needed, but I want to keep adding features and capabilities to this system, and the wireless and battery capabilities offer a lot of feature expansion. If I were simply installing the system depicted in the picture without the intention of adding to it, I might have opted for the less expensive Arduino Pro Mini.
Power is supplied to the microcontroller after the ignition switch, which, if functioning properly, should prevent the board from being powered up when the ignition switch is in the OFF position. This will keep the microcontroller from draining the car battery while the car is not in use and the battery is not being charged by the alternator. In the future, the onboard JST and LiPo charger of the Sparkfun Thing Plus could come in handy.
Now, I can’t just supply my Sparkfun Thing Plus with 12V from the ignition, so I’m using the Sparkfun Buck-Boost Converter to regulate that voltage down to 5V, which will then be routed to the Sparkfun Thing Plus’s VUSB pin. I will likely be placing a 1A or 500mA fuse between the 12V supply of the ignition and the Buck-Boost board. This should protect my ignition circuit in the chance that something I have added shorts.
From there I am utilizing the Sparkfun Qwiic Keypad – 12 Button as my HID device. This will live in the cabin of the car and will be used to enter the keycode. I’m connecting the keypad to my Thing Plus with a 100mm Qwiic Cable.
The next and most integral component is the Sparkfun Qwiic Single Relay. This board uses a ATTiny85 to act as an I2C slave and controls the the relay, allowing the user to open and close the relay using I2C communication. The Qwiic Relay will be acting as another switch on the starter solenoid power cable running from the ignition switch to the starter solenoid. When the relay is open, it should prevent current from reaching the starter solenoid. By controlling the current path to the starter solenoid, I can prevent the starter from engaging, and thus prevent the car from being started (in most cases).
Because this component will be under the hood, I opted to use some 22AWG wire to connect my Thing Plus to the Qwiic Relay. I will likely end up using some heat shielding on the wires and an enclosure for the Qwiic Relay to protect the parts from the heat of the engine bay and the elements.
I also want to include an option to bypass the Qwiic Relay. To do this, I’m going to use this toggle switch rated for 20A and 12V, which will be wired up in parallel with the Qwiic Relay on the starter solenoid control line.
Placing both the Qwiic Relay and the toggle switch under the hood should make hot-wiring the car much more difficult, requiring the would-be thief to go under the hood to reconnect the starter solenoid control line. Or just flip the switch... if they can find it.
At this point, it’s worth mentioning that I will be using at least 8AWG stranded wire to connect the Qwiic Relay and the toggle switch to the starter solenoid control line. This gauge of wire is large enough to safely handle the current of the starter solenoid control line, and should be available at any automotive parts store.
Above is a demo using a RedBoard Qwiic and a Qwiic Keypad to successfully close the Qwiic Relay when the proper keycode is entered. In this case the code is “1234.”
Below is the sketch I am using in the demo above:
#include <Wire.h>
#include "SparkFun_Qwiic_Keypad_Arduino_Library.h"
#define COMMAND_RELAY_OFF 0x00
#define COMMAND_RELAY_ON 0x01
const byte qwiicRelayAddress = 0x18; //Default Address
KEYPAD keypad1; //Create instance of this object
const char keyCode[] = {'1','2','3','4'}; //enter code here
char userEntry[] = {0, 0, 0, 0}; // used to store the presses coming in from user
boolean userIsActive = false; // used to know when a user is active and therefore we want to engage timeout stuff
#define TIMEOUT 30 // 100s of milliseconds, used to reset input. 30 equates to 3 second.
byte timeOutCounter = 0; // variable this is incremented to keep track of timeouts.
byte userEntryIndex = 0; // used to keep track of where we are in the userEntry, incremented on each press, reset on timeout.
#define stat_LED 13
void setup() {
Serial.begin(9600);
Wire.begin(); // join the I2C Bus
if (keypad1.begin() == false) // Note, using begin() like this will use default I2C address, 0x4B.
// You can pass begin() a different address like so: keypad1.begin(Wire, 0x4A).
{
Serial.println("Keypad does not appear to be connected. Please check wiring. Freezing...");
while (1);
}
testForRelayConnectivity();
relayOff();
pinMode(stat_LED,OUTPUT);
digitalWrite(stat_LED, HIGH);
delay(250);
digitalWrite(stat_LED, LOW);
Serial.println("Car Starter ready for operation!");
Serial.println("Keypad Car Starter Menu:");
}
void loop(void)
{
keypad1.updateFIFO(); // necessary for keypad to pull button from stack to readable register
char button = keypad1.getButton();
if (button == -1)
{
Serial.println("No keypad detected");
delay(1000);
}
else if (button != 0)
{
//Serial.print(button);
userEntry[userEntryIndex] = button; // store button into next spot in array, note, index is incremented later
printEntry();
userIsActive = true; // used to only timeout when user is active
if (checkEntry() == true)
{
relayOn();
digitalWrite(stat_LED, HIGH);
Serial.println("\n\r\n\rReady to start!");
clearEntry();
userIsActive = false; // don't display timeout stuff.
delay(1000);
digitalWrite(stat_LED,LOW);
}
userEntryIndex++;
if ( userEntryIndex == sizeof(keyCode)) userEntryIndex = 0; // reset
timeOutCounter = 0; // reset with any new presses.
}
delay(100); //10 is good, more is better, note this effects total timeout time
timeOutCounter++;
if ((timeOutCounter == TIMEOUT) && (userIsActive == true)) // this means the user is actively inputing
{
Serial.println("\n\r\n\rTimed out... try again.");
timeOutCounter = 0; // reset
userEntryIndex = 0; // reset
clearEntry();
//printEntry();
userIsActive = false; // so we don't continuously timeout while inactive.
}
}
boolean checkEntry()
{
for (byte i = 0 ; i < sizeof(keyCode) ; i++)
{
if (userEntry[i] == keyCode[i]); // do nothing, cause we're only looking for failures
else return false;
}
return true; // if we get here, all values were correct.
}
// "clear" entry with all spaces
void clearEntry()
{
for (byte i = 0 ; i < sizeof(userEntry) ; i++)
{
userEntry[i] = 0; // fill with spaces
}
}
void printEntry()
{
Serial.println();
Serial.print("UserEntry: ");
for (byte i = 0 ; i < sizeof(userEntry) ; i++)
{
Serial.print(char(userEntry[i]));
}
Serial.println();
}
// RelayOn() turns on the relay at the qwiicRelayAddress
// Checks to see if a slave is connected and prints a
// message to the Serial Monitor if no slave found.
void relayOn() {
Wire.beginTransmission(qwiicRelayAddress);
Wire.write(COMMAND_RELAY_ON);
Wire.endTransmission();
}
// RelayOff() turns off the relay at the qwiicRelayAddress
// Checks to see if a slave is connected and prints a
// message to the Serial Monitor if no slave found.
void relayOff() {
Wire.beginTransmission(qwiicRelayAddress);
Wire.write(COMMAND_RELAY_OFF);
Wire.endTransmission();
}
// testForConnectivity() checks for an ACK from an Relay. If no ACK
// program freezes and notifies user.
void testForRelayConnectivity() {
Wire.beginTransmission(qwiicRelayAddress);
//check here for an ACK from the slave, if no ack don't allow change?
if (Wire.endTransmission() != 0) {
Serial.println("Relay does not appear to be connected. Please check wiring. Freezing...");
while (1);
}
}
Maybe I'm overestimating the desire to steal this car? Nope, the desire is there... I see it in their eyes.
Stay tuned for part two, where I detail a step-by-step installation in the vehicle. In the meantime, let us know about hacks you have made on your vehicle, the issues you encountered and what you have planned next.