And now for new products! We'll start with the
LectroCandle Kit - the newest offering in our ever-increasing line of
kits. The LectroCandle kit is designed with the beginner in mind (it only requires through-hole soldering). This is essentially just what it sounds like - an electronic candle. It's comprised of 3 RGB LEDs that cycle through all the colors of the rainbow. Perfect to add a little brightness to your next project, or a great place to start for beginners!
Next, we have the
MintyBoost kit from
Adafruit Industries. This is a very cool kit that allows you to use a couple AA batteries to charge many devices over USB. Perfect for the electronics enthusiast on-the-go!
This is a
breakout board for the ISD1932,
a multiple-message record/playback device. This single chip can record
up to 64 seconds worth of voice messages. Microphone inputs and speaker
outputs are all handled by the ISD1932.
The
Serial Controlled Motor Driver
allows you to control up to two DC motors using a serial command
interface. The serial interface is easy to use and it lets the user
select an individual motor, the direction, and the desired speed
constant (up to 10 different speed from stop to full speed). The board
is based on the L298 Dual Full-Bridge Motor Driver from ST Micro. The
motor driver can provide up to 4 Amps of current to the motors (2 Amps
per motor). Great for precise control of your next robotics project!
Help your next project find its way with the
D2523T GPS Module.
The D2523T is a compact GPS smart-antenna engine board, which comes
equipped with a Sarantel GeoHelix high-gain active antenna and GPS
receiver circuits. The module is based around the high performance
50-channel u-blox 5 platform.
Here we have a 20mm rippled
wide optic lens. This is specifically designed for use with high intensity LEDs (like our
Rebel Luxeon LEDs). This lens will produce a rippled beam with a 24? beam angle.
So you want to use ultra-bright LEDs but don't want your project to melt? Good thinking. Check out this
heatsink designed for use with our
Rebel Luxeon LEDs. Keep your project cool!
More stuff to go along with the
Rebel Luxeon LEDs. This is a
Solderless LED Holder that snaps easily into the
heatsink above.
Now for the LEDs themselves! Available in
Royal Blue,
Red,
Cool White,
Green, and
Warm White. These are super-high intensity LEDs that are blindingly bright (seriously, please don't look right at them) and also are tiny (just about 3 x 4.5mm). Use them with the
heatsink and
holder above for a complete solderless LED casing.
The 7027 "BuckToot"
LED Power Module is a true constant current regulated driver for LEDs. Unlike standard power supplies, which deliver a fixed voltage to the output, the BuckToot LED driver is designed to reliably vary the output voltage as required to deliver a stable constant current to your LEDs.
This is a nice, simple toy DC motor for your next robotics project. This is a
small toy DC motor with about 29.5mm long leads. It has a small circular shaft which measures about 2.8mm long.
The
USB3318 is a high-speed USB 2.0 transceiver that supports system architectures based on a 13MHz reference clock. The USB3318 is an extremely flexible chip which allows the USB connector to act as a single port of connection for high speed data transfer, battery charging and stereo/mono audio accessories.

The
MMA7361LR1 is a low power, three-axis analog accelerometer. The sensor has a g-Select input which allows for the selection between two measuring ranges - ?1.5g or ?6g. There will be a breakout board coming soon!

This little guy (the
BMP085) is a ultra-low power barometric pressure sensor. It offers a measuring range of 300 to 1100 hPa with an absolute accuracy of down to 0.03 hPa. Perfect for your next weather-based project!
This
2xAAA battery holder puts a nice finishing touch on your battery powered project.
This holder features a sliding, removable cover as well as an ON/OFF switch which can be used to control power to your project.
The
MAX7219CNG is a compact, serial input/output common-cathode display driver that can interface microprocessors to 7-segment numeric LED displays of up to 8 digits, bar-graph displays, or 64 individual LEDs.