User Success Story: Cryologging the Cryosphere

When Adam Garbo of the Water and Ice Research Laboratory at Carleton University saw a lack of data coming from the cryosphere, he turned to an affordable, open-sourced solution he dubbed the Cryologger.

How to collect data on an moving glaciers in -40°C...

The Canadian Arctic is a fascinating and inhospitable place that remains an important area for science to study. In an environment undergoing rapid environmental change, there is an alarmingly small amount of data being collected – in part because of reliance on expensive and proprietary commercial data acquisition and telemetry systems. Scientist Adam Garbo knew there had to be a better way.

Focusing his research on “low-cost, open-source technology to help study the cryosphere,” Garbo set out to create an affordable and open-source solution to this deficiency of data. This is the idea behind the Cryologger. Configured for a number of different research applications, such as an iceberg tracking beacon, an automatic weather station, and most recently, a glacier velocity measurement system, the Cryologger is a flexible and powerful tool.

SparkFun's Artemis Global Tracker being used for research applications in the Canadian Arctic

Learn more about Garbo's project and follow his beacons progress as they move through the Arctic here.

SparkFun GPS-RTK-SMA Breakout - ZED-F9P (Qwiic)

GPS-16481
$259.95