SparkFun now has limited stock of Arduino's latest board!
We have a very special announcement for today's blog: The Arduino Uno Mini Limited Edition is now available at SparkFun Electronics, but only in a small batch! Featuring similar specs to the full-sized Uno and based on the ATMega328 microcontroller, this board is just as capable and is a neat memento for those of us who love the board and brand.
In addition to the classic microcontroller, the board features 14 digital pins and six analog, just like the full sized Uno. It also uses 5V logic and has six PWM pins too! The biggest difference besides size is the use of a USB Type C Connector instead of the classic USB-B.
Please be aware that due to expected demand and its limited nature, there is a limit of two boards per customer for the Arduino Uno Mini.