Pi 5 & Arduino Friday Double-Header!

We have so many products from our friends at Raspberry Pi and Arduino for you to check out today!

Hello hello and welcome to another Friday Product Post here at SparkFun Electronics! As you may have noticed yesterday, Raspberry Pi announced their new Raspberry Pi 5 boards and several new accessories that go along with them. These boards come in 4GB and 8GB versions that are sure to appease your desktop computer and development project needs! Following that, we have three new boards from Arduino! Two new Nano boards that feature the popular ESP32 (you just have to decide whether or not your headers are already soldered on or not) and their new version of the Mega and Due, the Giga R1! Let's jump in and take a closer look at all of this week's new products!

Learn how the new Raspberry Pi 5 compares to the previous iteration!

Raspberry Pi 5 - 4GB

DEV-23550
$110.00

Raspberry Pi 5 - 8GB

DEV-23551
$180.00

The next iteration of the Raspberry Pi single board computer featuring a 64-bit quad-core Arm Cortex-A76 processor running at 2.4GHz, Raspberry Pi 5 4GB and 8GB delivers a 2–3× increase in CPU performance relative to Raspberry Pi 4. Alongside a substantial uplift in graphics performance from an 800MHz VideoCore VII GPU; dual 4Kp60 display output over HDMI; and state-of-the-art camera support from a rearchitected Raspberry Pi Image Signal Processor, it provides a smooth desktop experience for consumers, and opens the door to new applications for industrial customers.


Raspberry Pi 5 Basic Kit - 4GB

KIT-23616
Retired

Raspberry Pi 5 Basic Kit - 8GB

KIT-23617
Retired

These are basic kits in 4GB and 8GB versions for getting started with the Raspberry Pi 5. Included in the kit is a new power supply that meets the power needs for the 5. It also includes our choice for a microSD card for use with the Pi line that meets the specs set by the Raspberry Pi Foundation and has fantastic read/write speeds. In addition a MicroHDMI cable is included for interfacing an HDMI display with the Pi 5 and We've also thrown in our Qwiic Shim for Raspberry Pi, the quickest way to use I2C devices with the Raspberry Pi.


Arduino Giga R1 WiFi

WRL-23319
$72.82 $65.54

The Arduino GIGA R1 WiFi is designed for ambitious makers who want to step up their game. It levels the playing field for gamers, artists, sound designers and anyone coming to the tech world with big ideas on a budget – because it packs advanced features into an accessible component, with the same form factor as our popular Mega and Due.


Arduino Nano ESP32

DEV-23320
$20.00

Arduino Nano ESP32 with Headers

DEV-23321
$21.00

Introducing the Nano ESP32 (with headers included or soldered on), a powerful addition to the Arduino ecosystem that brings the popular ESP32-S3 to the world of Arduino and MicroPython programming. Whether you're a beginner stepping into the world of IoT or MicroPython, or an advanced user looking to incorporate it into your next product, the Nano ESP32 is the perfect choice. It covers all your needs to kick-start your IoT or MicroPython project with ease.


Raspberry Pi 5 Case - Red/White

PRT-23587
$12.05

The Raspberry Pi 5 case is a refinement of the Raspberry Pi 4 case. With improved thermal features to support the higher peak power consumption of Raspberry Pi 5, it integrates a variable-speed fan. The fan is powered and controlled from a dedicated connector on the Raspberry Pi 5 PCB.


Raspberry Pi Active Cooler

PRT-23585
$15.00

The Raspberry Pi Active Cooler provides an alternative cooling solution for users who wish to use their Raspberry Pi 5 under sustained heavy load without a case. It combines a large metal heatsink with a variable-speed blower, again powered and controlled via the fan connector, and attaches to the Raspberry Pi 5 PCB via sprung pins into a pair of mounting holes.


Raspberry Pi 27W USB-C PD Power Supply - White

TOL-23583
$17.25

Raspberry Pi 27W USB-C PD Power Supply - Black

TOL-23584
$17.25

The white or black Raspberry Pi 27W USB-C PD (Power Delivery) Power Supply will deliver a maximum of 5.1V, 5A enabling the Raspberry Pi 5 to power a wider range of peripherals. The total power drawn from the four USB ports on Raspberry Pi 5 is limited by default to a nominal 600mA; this limit is automatically increased to a nominal 1.6A when the USB-C PD Power Supply is detected.


Raspberry Pi 5 Display Cable - 200mm

PRT-23683
$2.50

Raspberry Pi 5 Camera Cable - 200mm

PRT-23682
$2.50

These are 200mm display and camera cables for use with MIPI displays and the Raspberry Pi 5. The Raspberry Pi 5 provides two four-lane MIPI connectors, each of which can support either a camera or a display. These connectors use the same 22-way, 0.5mm-pitch “mini” FPC format as the Compute Module Development Kit, and require adapter cables to connect to the 15-way, 1mm-pitch “standard” format connectors on our current camera and display products.


Edimax 2-in-1 Wi-Fi 4 N150 & Bluetooth® 4.2 Nano USB Adapter

WRL-22824
$12.99

The Edimax 2-in-1 Wi-Fi 4 N150 & Bluetooth® 4.2 Nano USB Adapter is a nano-sized USB Wi-Fi adapter with Bluetooth® 4.2 that supports Wi-Fi up to 150Mbps while allowing users to connect to all the latest Bluetooth® devices such as mobile phones, tablets, mice, keyboards, printers and more. Supporting the latest Bluetooth® 4.2 version, this adapter offers ultra-low power consumption with Bluetooth® Low Energy (BLE) while transferring data or connecting devices.


That's it for this week. As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there, be kind to one another! We'll be back with more new products next week so make sure to check back then. Happy hacking!

Never miss a new product!