Meet the New Digi XBee®

The newest Digi XBee® modules are now available at SparkFun Electronics, and we have new boards to support them!

You know as well as we do, that if we are announcing a new product on a day other than Friday, it's a big deal! We consider our friends at Digi International some of our closest and oldest, so when they approached us about supporting their new Digi XBee® modules with revised versions of our classic Explorers and development boards, we couldn't say no! Today, we are happy to announce four brand new boards and a new kit, each designed from the ground up to support The Digi XBee RR and GNSS modules as well as all legacy, through-hole modules that have been released in the past. Let's jump in and take a closer look at our new boards and the new Digi XBee modules!

SparkFun Digi XBee® Development Board

WRL-21636
$22.95

The SparkFun Digi XBee® Development Board is designed to help you quickly and easily prototype low-power cellular IoT applications using the new Digi XBee 3 Low-Power LTE-M/NB-IoT, Digi XBee RR, and any existing through-hole Digi Xbee module. This board breaks out all the functionality of your XBee module and adds the ability to connect to the cellular network and (drumroll, please) GNSS.


SparkFun Digi XBee® Explorer Regulated

WRL-22032
$14.50

Unleash the power of Digi XBee® modules with the next-gen SparkFun Digi XBee® Explorer Regulated! This versatile breakout board bypasses a USB-C connection, packing all the XBee functionality you need alongside the power of Digi's newest XBee 3 modules (XBee 3 LTE-M/NB-IoT and XBee RR Pro) into a single, convenient solution. The SparkFun Digi XBee® Explorer Regulated is the perfect companion for any low-power cellular IoT project. Its simplicity, versatility, and robust features make it ideal for beginners and seasoned developers.


SparkFun Digi XBee® Explorer USB-C

WRL-22043
$19.50

Unleash the power of Digi XBee® modules with the next-gen SparkFun Digi XBee® Explorer USB-C! This compact, easy-to-use adapter is the perfect bridge between your computer and any through-hole Digi XBee module, making prototyping and development a breeze. Whether you're a seasoned IoT architect or just starting your wireless journey, the Digi XBee® Explorer USB-C empowers you to bring your ideas to life.


SparkFun Digi XBee® Arduino Shield - USB-C (Qwiic)

WRL-22131
$13.95

The Sparkfun Digi XBee® Arduino Shield is your gateway to a world of wireless innovation on your favorite Arduino device. This shield integrates Digi's cutting-edge XBee 3 Low-Power LTE-M/NB-IoT and Digi XBee RR Pro modules (or any existing through-hole Digi XBee module) with your trusty Arduino, empowering you to build wireless projects that reach further and do more than ever. Whether you're a seasoned developer or a curious beginner, the SparkFun Digi XBee® Arduino Shield - USB-C (Qwiic) empowers you to bring your wildest IoT ideas to life.


SparkFun Digi XBee® Cellular Kit

KIT-24441
$139.95

The SparkFun Digi XBee® Kit is your ticket to remote sensing adventures. Unbox this treasure trove of tools and watch your imagination take flight. Included with this kit, you will find everything you need to get started using Digi XBee and the Qwiic Connect System.


Digi XBee 3 Low-Power LTE-M/NB-IoT, GNSS, no SIM

WRL-22329
$75.95

The Digi XBee 3 global cellular module is a cutting-edge, compact module engineered for rapid integration of cellular IoT capabilities. This innovative solution is equipped with cellular and BLE connectivity with end-device carrier certifications, and is designed to create secure wireless devices featuring global connectivity and positioning capabilities. A combination of the XBee ecosystem and cellular functionality makes for a simple system for working with data over a cellular connection.


Digi XBee 3 North America LTE Cat 1, 3G, GNSS, no SIM

WRL-22330
$116.95

The Digi XBee 3 global cellular module is a compact, programmable, reliable solution with BLE and end-device carrier certifications for developing secure wireless devices with worldwide connectivity and global positioning. A combination of the XBee ecosystem and cellular functionality makes for a simple system for working with data over a cellular connection.


Digi XBee® RR Pro Module - SMA Antenna

WRL-22631
$38.95

Digi XBee® RR Module - SMA Antenna

WRL-22630
$23.95

XBee RR 802.15.4 RF Modules (available in Pro and non-Pro versions) are embedded solutions providing wireless end-point connectivity to devices. These devices use the IEEE 802.15.4 networking protocol for fast point-to-multipoint or peer-to-peer networking. They are designed for high-throughput applications requiring low latency and predictable communication timing. The XBee RR 802.15.4 RF Module supports the needs of low-cost, low-power wireless sensor networks. The devices require minimal power and provide reliable delivery of data between devices. The devices operate within the ISM 2.4 GHz frequency band. It allows local configuration with BLE using the Digi XBee Mobile app. The XBee RR is functionally equivalent to the XBee3 but does not offer the MicroPython nor the full BLE programmable services offered by the XBee3.


Digi XBee® RR Pro Module - U.FL Antenna

WRL-22629
$38.95

Digi XBee® RR Module - U.FL Antenna

WRL-22628
$23.95

XBee RR 802.15.4 RF Modules (available in Pro and non-Pro versions) are embedded solutions providing wireless end-point connectivity to devices. These devices use the IEEE 802.15.4 networking protocol for fast point-to-multipoint or peer-to-peer networking. They are designed for high-throughput applications requiring low latency and predictable communication timing. The XBee RR 802.15.4 RF Module supports the needs of low-cost, low-power wireless sensor networks. The devices require minimal power and provide reliable delivery of data between devices. The devices operate within the ISM 2.4 GHz frequency band. It allows local configuration with BLE using the Digi XBee Mobile app. The XBee RR is functionally equivalent to the XBee3 but does not offer the MicroPython nor the full BLE programmable services offered by the XBee3.


And that's it! If you happen to be at CES this week, make sure to hit up Chris if you have any questions, comments, or concerns you may have. Otherwise, we'll talk with you this Friday to go over all our new products for the week! See you then and happy hacking!