Use LoRa to Get Better RTK Accuracy... From 9 Miles Away!

How far can you push RTK corrections using LoRa? In our new video, we test a long-range base and rover setup using the SparkPNT Facet with a built-in 915MHz, 1W LoRa radio, achieving reliable RTK accuracy over miles of line-of-sight distance.

Getting GNSS corrections relies on connectivity, which can be limiting. Luckily, you can go long range with the Facet FP. These devices are LoRa-compatible and even come with an antenna.

Check out how it works in our newest video, where Nate uses a Facet FP with LoRa to get great RTK accuracy 9 miles away from our correction source.

We demonstrate a real-world setup transmitting corrections from a base station positioned on a known survey mount to a rover nearly 9 miles away, while maintaining centimeter-level accuracy.

  • LoRa enables long-range correction transmission without internet
  • RTK fixes can be maintained even with intermittent packet delivery
  • Line-of-sight plays a critical role in performance
  • Built-in radios simplify base + rover deployments in the field

The Facet FP line of receivers are repairable, user-upgradeable, and use open-source firmware. Learn more about them here: