Two new IoT RedBoards are now available, each featuring the new P4X processor from Espressif!
Hello everyone and welcome back to another Friday Product Post! We hope you all had a happy and safe Halloween! We're very excited to announce our new products today, because we have two new IoT RedBoards that feature Espressif's ESP32-P4 (specifically using the v3 version, the P4X)! It'll be up to you, however, to choose between a wireless version with an on-board ESP32-C5 co-processor or a wired version via PoE! Following that we have a Lightning Arrester from SparkPNT moving over to the SparkFun catalog.
Before we get to this week's new products, a quick reminder: Our November Deals sales event is currently live with 30% off select sensors! Additionally, this Monday, November 9th, we will be entering the second week of deals with sales on some of our most popular GPS/GNSS Devices and Accessories. Each week, we put a new set of SparkFun Original products on sale to help you prepare for the holiday season, or if you simply want to save a few bucks and get something for yourself. Get an early look today and head over to the November Deals page to plan your sales shopping!
The SparkFun ESP32-P4 & ESP32-C5 IoT RedBoard is a high-performance development board designed for demanding edge computing and human-machine interfacing (HMI) applications. By pairing the processing power of Espressif's ESP32-P4 with the wireless networking of the ESP32-C5 WROOM module, this RedBoard provides a foundation for custom touch displays, camera integration, and advanced IoT projects that require reliable security features.
At the heart of these boards lies the ESP32-P4NRW32X (or P4X), an upgraded dual-core RISC-V processor running at up to 400MHz for intensive tasks like image and voice processing. The P4X also includes an integrated low-power RISC-V core that runs at up to 40MHz for standby operations, and brings advanced memory subsystems directly to your workbench. Best of all, it boasts 32MB of PSRAM, Direct Memory Access (DMA) controllers, and AI instruction extensions to handle massive datasets without bogging down the system!
Instead of relying on wireless modules, this version of the ESP32-P4 IoT RedBoard integrates a PoE circuit to provide both network connectivity and power through a single cable. The board's MagJack RJ45 connector provides a dedicated 10/100Mbps Ethernet transceiver that handles wired data transmission. Because PoE power delivery is a major safety concern, we've included a built-in 5V/1.8A buck regulator that safely steps down the PoE voltage to power the main board and any connected peripherals.
When properly installed, this Lightning Arrester helps prevent lightning strikes to the antenna from damaging the attached equipment. Additionally, SMA connections allow the arrester to be placed in-line with the antenna cable.
That's it for this week! If you aren't already a subscriber to our New Product Newsletter, you really should be. As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there and be kind to one another! Happy hacking!