New Product Friday: The Build Upons

Some unique LEDs, a teensy little development board, and a new FEZ kit. That's what's new this week.

Hello again. This week we have a few products and a couple product-specific videos. Don't worry, the Friday New Product Post Video didn't go away, we just did individual videos again this week. Let's get right to it, here are the products for this week.

Build Upons LED - PTH (10 Pack)

COM-13312
Retired

Wouldn't it be cool if you could integrate LEDs into your Danish-made interchangeable plastic building block system? The Build Upons let you do exactly that! They snap directly into your favorite name-brand building bricks and work like a normal LED. Each 10 pack comes with 2 of each of 5 colors. Want to see them in action? Check out this video:

Teensy LC

DEV-13305
Retired

The Teensy LC is a breadboard-friendly development board with loads of features in a, well, teensy package. The LC is a low cost version of the popular Teensy that has a lot of the same features, but at a lower price. The processor on the Teensy also has access to the USB and can emulate any kind of USB device you need it to be, making it great for USB-MIDI and other HID projects. The 32 bit processor brings a few other features to the table as well, such as multiple channels of Direct Memory Access and an I2S digital audio interface! There are also 4 separate interval timers plus a delay timer! It's a cool little board.

FEZ Spider Tinker Kit

DEV-13306
Retired

The FEZ Spider Tinker Kit is a 100% open-source (hardware and software) .NET Gadgeteer compatible mainboard running .NET Micro Framework. This tinker kit enables users to program the FEZ Spider and its add-on modules from Microsoft’s Visual Studio using C# or Visual Basic, allowing developers to take advantage of the extensive built-in libraries for networking, file systems, graphical interfaces, and peripherals. Nick put together a little demo and explains what's included in the kit. Let's watch.

Classic Nick. That's it for this week. We'll be back again next week with more new stuff, so be sure to check back then. Thanks for reading and watching.