Friday Product Post: Tool Time (Pt.1)

Soldering tools! Tons and tons of soldering tools! Enjoy!

Welcome back, everyone! We hope you are in need of some new soldering tools because we have top-quality options in store for you today. A new soldering station, butane soldering iron, soldering tips and a couple of workbench items that will make your life so much simpler! We don't have a product video this week, as there are so many new products to cover. So without further ado, let's just dive in!

Weller WLC100 Soldering Station

TOL-14228
Retired

The WLC100 from Weller is a versatile 5 watt to 40 watt soldering station that is perfect for hobbyists, DIYers and students. The WLC100 operates at 120V and features a five-position dial to provide variable power control to the soldering station. The included 40 watt "pencil" soldering iron is lightweight with a cushioned foam grip and an interchangeable flat ST3 tip. The soldering iron can even be detached for your on-the-go soldering needs!

Weller Portasol Butane Soldering Iron Kit

TOL-14226
Retired

The Weller Portasol Kit is a fantastic box filled with a pocket-sized, butane-powered soldering iron as well as multiple attachments for it. Each soldering iron has been equipped with a push-button Piezo ignition that adjusts from 25-Watt to 75-Watt for ease and convenience. This iron is versatile too, functioning as a soldering iron, hot air gun, butane torch or hot knife --- you'll be hard pressed to find something you can't do! They're ready to use quickly --- fewer than 40 seconds after ignition --- and can run for up to 60 minutes on a single tank of butane.

Solder-Mate Solder Dispenser

TOL-14232
Retired

The Solder-Mate™ Solder Dispenser provides you with an easy way to, well...dispense solder! This handy tool provides a continuous supply of solder (until the roll runs out, that is), freeing up hand space and minimizing downtime. Each solder dispenser can hold up to a one-pound solder spool, which you will need to supply yourself. If you need some solder (like that pictured above) we have quarter-pound spools of lead-free solder in 0.032" (0.8mm) and 0.020" (0.5mm) diameters.

Solder Tip Polishing Bar

TOL-14233
Retired

Do you need to remove the oxidation and surface contamination from your soldering iron tip? The Solder Tip Polishing Bar allows you to do just that! This bar provides a great way to bring your older or neglected soldering tips back from the dead.

And speaking of soldering iron tips...

Soldering Tip - Weller - Standard (ST1)

TOL-14229
Retired

We have four new soldering iron tips for our two new irons today! The standard ST1 tip for the WLC100...

Soldering Tip - Weller - Flat (ST3)

TOL-14230
Retired

The flat ST3 tip for the WLC100...

Soldering Tip - Weller - Conical (ST6)

TOL-14231
Retired

The "conical" ST6 tip for the WLC100...

Butane Soldering Tip - Weller - Double Flat (1.0mm)

TOL-14227
Retired

And finally the double flat tip for the P2KC butane iron.

Alright folks, that's it for this week. As this post's name suggests, this is only the first week of new tool products, so be sure to check out even more new tools next Friday! As always, we can't wait to see what you make with them! Shoot us a tweet @sparkfun, or let us know on Instagram or Facebook. We’d love to see what projects you’ve made!

We'll see you next Friday!