Arduino Day Deals End Tonight!
Take 20% off most SparkFun Original boards today!
Blink and you may have missed it, but Arduino Day was Saturday, 3/16. To celebrate the fact SparkFun probably wouldn't be here without Arduino, we've taken 20% off most of our SparkFun Original boards! We aren't a big fan of leaving discounts just to the weekend though, so we've extended our deals through the end of today. Check out some of our favorites on sale below, but act fast as some boards may sell out. You have until 11:59 p.m. MST tonight to score a deal. Happy belated Arduino Day!
SEN-15050
The SparkFun Triad Spectroscopy Sensor is a powerful optical inspection sensor with three sensors combined alongside LEDs us…
DEV-12640
Here at SparkFun, we refuse to leave 'good enough' alone. That's why we're adding to our line-up of Arduino-compatible microc…
WIG-13660
The WAV Trigger is a unique high-fidelity polyphonic audio player with surprising capabilities.
SEN-13879
The SparkFun Load Cell Amplifier is a small breakout board for the HX711 IC that allows you to easily read load cells to meas…
DEV-13712
The SparkFun OpenLog can store, or "log", huge amounts of serial data and act as a black box of sorts.
WRL-13225
The SparkFun XBee Explorer Serial is a simple to use, RS232 to serial base unit for the XBee line.
SEN-13676
The SparkFun BME280 Atmospheric Sensor Breakout is the easy way to measure barometric pressure, humidity, and temperature rea…
ROB-12779
The EasyDriver is a simple to use stepper motor driver, compatible with anything that can output a digital 0 to 5V or 0 to 3.…
DEV-09716
This is a basic breakout board for the FTDI FT232RL USB to serial IC. The pinout of this board matches the FTDI cable to work…
DEV-13907
The SparkFun ESP32 Thing is a comprehensive development platform for Espressif’s ESP32, their super-charged version of the …
WRL-15006
The SparkFun 1-Channel LoRa Gateway is a powerful 3-network capable device thanks to an onboard ESP32 WROOM module and an RFM…
Retired
SEN-14001
The SparkFun 9DoF Razor IMU M0 combines a SAMD21 microprocessor with an MPU-9250 9DoF (9 Degrees of Freedom) sensor to create…
Retired