Mighty Modular Power Processors

Two huge releases happened this week with SparkFun MicroMod and Raspberry Pi Compute Module 4. Let's take a look!

Hello there, everyone! We have had a very busy week here with two major product releases: On Monday, Raspberry Pi released their new Compute Module 4 series and, since we are now an Approved Reseller, we are offering several different options of the board including a way to easily access them. On Wednesday, we announced our brand new SparkFun MicroMod ecosystem that allows you to swap out small Processor Boards on function-specific Carrier Boards. Let's take a closer look!

Watch Avra build a project with our new MicroMod boards!

SparkFun MicroMod Artemis Processor

DEV-16401
$17.50

SparkFun MicroMod ESP32 Processor

WRL-16781
$19.95

SparkFun MicroMod SAMD51 Processor

DEV-16791
Retired

Pick processors from SparkFun's own Artemis to ESP32 or SAMD51 (and more to come). Mix, match, test and prototype different processors with few to no code changes!

  • SparkFun MicroMod Artemis Processor: Leveraging the ultra powerful Artemis Module, the SparkFun MicroMod Artemis Processor is the brain board of your dreams. With a Cortex-M4F with BLE 5.0 running up to 96MHz, and with as low power as 6uA per MHz (less than 5mW), the M.2 MicroMod connector allows you to plug in a MicroMod carrier board with any number of peripherals.
  • SparkFun MicroMod ESP32 Processor: The MicroMod ESP32 Processor Board combines Espressif's ESP32 with our M.2 connector interface to bring a processor board with reliable WiFi and Bluetooth capabilities into our MicroMod ecosystem.
  • SparkFun MicroMod SAMD51 Processor: With a 32-bit ARM Cortex-M4F MCU, the SparkFun MicroMod SAMD51 Processor Board is one powerful microcontroller packaged on a small board! The provides you with an economical and easy-to-use development platform if you need more power with minimal working space.

Rob goes over the MicroMod ecosystem boards in more detail!

SparkFun MicroMod ATP Carrier Board

DEV-16885
$20.50

SparkFun MicroMod Input and Display Carrier Board

DEV-16985
$61.50

SparkFun MicroMod Data Logging Carrier Board

DEV-16829
$22.95

SparkFun MicroMod Machine Learning Carrier Board

DEV-16400
$22.95

Choose a carrier board to access different inputs and outputs based on your specific needs. Each carrier board is easily expandable by utilizing our Qwiic Connect System.

  • SparkFun MicroMod ATP Carrier Board: Access all the pins (i.e. ATP) of the MicroMod processor boards with the SparkFun MicroMod ATP Carrier Board! This board breaks out the MicroMod processor board's pins on the M.2 connector to 0.1-inch spaced female headers and PTH pads on the edge of the board.
  • SparkFun MicroMod Input and Display Carrier Board: This carrier board combines a 2.4-inch TFT display, six addressable LEDs, onboard voltage regulator, a 6-pin IO connector, and microSD slot with the M.2 pin connector slot, so it can be used with compatible processor boards in our MicroMod ecosystem.
  • SparkFun MicroMod Data Logging Carrier Board: The SparkFun MicroMod Data Logging Board offers a highly customizable, low-power data logging platform using the MicroMod system, allowing you to choose your own processor to pair with the carrier board.
  • SparkFun MicroMod Machine Learning Carrier Board:The MicroMod Machine Learning Carrier Board combines some of the features of our SparkFun Edge Board and SparkFun Artemis boards, but allows you the freedom to explore with any processor in the MicroMod lineup without the need for a central computer or web connection. Voice recognition, always-on voice commands, gesture, or image recognition are possible with TensorFlow applications.

Raspberry Pi Compute Module 4 32GB (Wireless Version) - 4GB RAM

DEV-17392
$110.00

Raspberry Pi Compute Module 4 Lite (Wireless Version) - 2GB RAM

DEV-17384
$55.00

Raspberry Pi Compute Module 4 8GB - 2GB RAM

DEV-17284
$65.00

Raspberry Pi Compute Module 4 8GB (Wireless Version) - 2GB RAM

DEV-17391
$80.00

Raspberry Pi Compute Module 4 16GB - 2GB RAM

DEV-17390
$70.00

Raspberry Pi Compute Module 4 - Lite

DEV-17364
$45.00

Raspberry Pi Compute Module 4 I/O Board

DEV-17360
$38.50

Raspberry Pi 4 Compute Module Antenna Kit

WRL-17389
$15.00

Since we are now an Approved Reseller for Raspberry Pi, we are happy to carry versions of the brand new Raspberry Pi Compute Module 4. The Raspberry Pi Compute Module 4 represents a huge change for the Compute Module line, the biggest change being the move from the DDR2 SODIMM connector form factor to a high density connector on the bottom of the board. True to the line, the Compute Module 4 packs all the best features of the Raspberry Pi Model B 4 into a more favorable form-factor for embedded or OEM applications.


That's it for this week! As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram or Facebook. We’d love to see what projects you’ve made!

Never miss a new product!