Survey the Brobdingnagian Wilds

The new SparkFun RTK Surveyor is now available from SparkX, along with a new RPi4 Case Fan, Teensy 4 SmartLED Shield, and M6E-NANO RFID Module.

Hello everyone and welcome back to another Friday Product Post. If you celebrated Thanksgiving last week, we hope you were safe and ate a ton of turkey and maybe scored a few amazing sales during Black Friday and Cyber Monday. This week we have several new products to show off, and it all starts with the new SparkFun RTK Surveyor. This pre-programmed, ready-to-use GNSS/GPS product is now available for all of your surveying needs at a fraction of the price of other options on the market. Following that, we started carrying the new Raspberry Pi 4 Case Fan, the new Teensy 4 SmartLED Shield, and M9E-NANO RFID Module.

If you're curious when you'll need to get your order before the holidays, make sure to check out our Holiday Shipping 2020 page.

Now, let's take a closer look at all of our new products!

We're going to name ours "Tyler, The Surveyor"

SparkFun RTK Surveyor

SPX-17369
Retired

The SparkFun RTK Surveyor is an easy to use GNSS receiver for centimeter-level positioning. Perfect for surveying, this preprogrammed device can also be used for autonomous driving, navigation, asset tracking and any other application where there is a clear view of the sky. The RTK Surveyor can also be used as a base station. With the flick of a switch, two RTK Surveyors can be used to create an RTK system capable of 14 mm horizontal positional accuracy. The built-in Bluetooth connection via an ESP32 WROOM enables the user to use the RTK Surveyor with their choice of GIS application on a phone or tablet. The built in battery allows field use for up to four hours, and is compatible with common USB battery banks.


Raspberry Pi 4 Case Fan

PRT-17368
$5.80

The Raspberry Pi 4 Case Fan works with Raspberry Pi 4 and the Raspberry Pi 4 Case. Designed for overclockers and other power users, it keeps your Raspberry Pi 4 at a comfortable operating temperature even under heavy load.


SmartLED Shield - Teensy 4

DEV-17521
Retired

The SmartLED Shield enables a Teensy 4 to drive high-quality graphics to HUB75 RGB LED panels, with 36-bit color and 240 Hz refresh rate across large panels (e.g. 128x64 pixels). A Teensy 4.0 or Teensy 4.1 with pins fits into the socket on the shield, and the shield can attach directly to the HUB75 panel or through a ribbon cable. The SmartMatrix library for Arduino makes it easy to draw basic graphics, create scrolling and static text, draw beautiful patterns using FastLED, and play animated GIFs on the panel.


RFID Module - M6E-NANO

SEN-16887
Retired

The M6E-Nano RFID Module delivers a small form factor embedded UHF RFID option with very low power consumption and is ideal for battery operated, low cost, small form-factor portable readers. The M6E-Nano’s wide RF output range (0 dBm to +27 dBm) is important for the read/write requirements for RFID-enabled printers and tag commissioning stations.


That's it for this week! As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram or Facebook. We’d love to see what projects you’ve made! Please be safe out there, be kind to one another, and have a great weekend!

Never miss a new product!