Surprise, One Last Flash Sale!
All good things must come to an end. We’re calling it a wrap on holiday sales with one last Flash Sale - 25% off select MicroMod boards. Available through Weds, Dec 8 @ 10 a.m. MST.
Surprise! We’re running one last Flash Sale for the Holiday 2021 season! Now through Weds, Dec 8 at 10 a.m. MST, we’re taking 25% off select MicroMod boards. Boards part of this Flash Sale are below. Rules and information are listed beneath the products.
As a reminder, be sure to grab those last minute gifts or project items soon if you need them in time for December 24th. Today is the deadline for Economy Ground and this Thursday is the deadline for Ground shipping. More details on holiday shipping guidelines can be found here.
Here are the deals!
DEV-16402
This board leverages the awesome computing power of the NXP iMXRT1062 chip (ARM Cortex-M7) and pairs it with the M.2 MicroMod…
DEV-16829
The MicroMod Data Logging Carrier offers a low-power data logging platform using the MicroMod system allowing you to choose y…
DEV-17724
The Double MicroMod Qwiic Carrier Board can be used to rapidly prototype with other Qwiic devices.
DEV-16401
Featuring the Artemis Module, this processor is capable of machine learning, Bluetooth, I2C, GPIO, PWM, SPI & packaged to fit…
DEV-17723
The Single MicroMod Qwiic Carrier Board can be used to rapidly prototype with other Qwiic devices.
DEV-17725
The Update Tool also makes it simple to communicate directly with the SARA using u-blox’s sophisticated m-center cellular e…
DEV-16985
Add data, input, & visibility to your project with a 2.4" TFT display, 6 addressable LEDs, onboard voltage regulator, 6 pin I…
DEV-16400
The MicroMod Machine Learning Carrier combines the freedom to explore any processor in the MicroMod lineup without the need f…
Rules & Information for Flash Sale:
- Flash sale will run from 10 a.m. MST Tues, Dec 7, 2021 through 10 a.m. MST Weds, Dec 8, 2021.
- No rainchecks or backorders will be allowed.
- We will not be allowing the combining of orders during this sale.
- Distributor and reseller accounts will not be eligible for sale prices unless specifically noted otherwise.
Please note: We will be working hard to ship as many orders as quickly as possible, but we cannot guarantee same-day shipping for sale orders. Please allow additional days for sale orders to ship due to increased volume.