Easy Listening

We are working on a lot of products behind the scenes so we are taking it a little easy with this week's Product Post!

Hello all and welcome back to another Friday Product Post here at SparkFun Electronics! It's the last full week of August and we are hard at work with a lot of new boards that will be releasing in the coming weeks and months. In lieu of that, we have a bit of a lighter Friday post for you, with only two component products. The first of which is a compact, Wide Frequency Range Speaker option for your next audio project. Following that, we have a spool of two-conductor Hook-up Wire that can easily be used on any workbench or project station. And that's it! With that, let's jump in and take a closer look at both of this week's new products!

Wide Frequency Range Speaker - 3in. (Polypropylene Cone)

COM-18379
Retired

This wide range speaker is an excellent choice for compact applications requiring high fidelity music, or high intelligibility voice/communications audio. A talc-filled, polypropylene cone with a rubber surround allows this driver to be used either indoors or outdoors.


Hook-up Wire 2-Conductor - Clear (22AWG-7x30, Stranded, 25ft)

PRT-18382
$5.95

This standard 22 AWG hook-up wire is great for general connections between projects (low or high current applications). When you only need two connections to something (like power, a button or an indicator LED), this keeps your wiring nice and organized. It is also commonly used as speaker wire to connect from your speaker amp to the speakers.


And that's it! Like we said, a pretty easy week, for sure. As always, we can't wait to see what you make. Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there, be kind to one another, and we'll see you next week with even more new products!

Never miss a new product!