ACTUAL CO2 Measurements, Not Estimated!

This week, we're introducing a new CO2 Combo Sensor featuring Sensirion's STCC4 and SHT40 environmental sensors!

Welcome back, one and all, to another Friday Product Post here at SparkFun Electronics! This week, we have two new products to show you; the first features two new environmental sensors from our friends at Sensirion. The new SparkFun Qwiic CO2 Sensor features the STCC4 CO2 sensor and the SHT40 digital humidity and temperature sensor, giving you a way to measure actual CO2 concentrations, whereas pretty much every other sensor in its field only measures estimated levels. Following that, we have a new UHF RFID H9 Tag. This paper-thin, adhesive tag can stick to practically anything and delivers everything the previous version did in a slightly larger package. Ready to take a closer look? Let's go!

Deal of the Week: SparkFun RedBoard Turbo - SAMD21 Development Board now 47% Off

This Week's New Products:

SparkFun CO2 Sensor - STCC4/SHT40 (Qwiic)

SEN-31536
$30.95

The SparkFun STCC4/SHT40 Qwiic CO2 Sensor is a simple indoor air quality breakout that primarily measures CO2 concentration, as well as temperature and relative humidity, over I2C. Specifically, the board features a pair of Sensirion sensors, isolated in their own section: the STCC4 CO2 sensor and the SHT40 digital temperature and humidity sensor. These two sensors work together to output precise and environmentally compensated CO2 readings without any complicated wiring.

While most CO2 sensors measure estimated CO2 concentration, the STCC4 uses thermal conductivity to directly measure actual CO2 concentrations from 400 to 5000 ppm (parts per million) with an accuracy of ±100ppm + 10% of the total reading. It outputs a calibrated digital signal that works with temperature and humidity data sent to it by the SHT40.


UHF RFID H9 Tag - 70mm x 20mm (Adhesive)

WRL-31965
$1.25

This paper-thin, adhesive UHF RFID tag has been designed for versatility and high performance. Measuring just 70mm x 20mm, it's small enough to stick to almost any object while still providing reliable wireless identification. Each tag is built around the H9 RFID chip, which offers significant upgrades in speed, range, and memory over the standard H3 generation.


This Week's New Price Drop:

SparkFun Indoor Air Quality Combo Sensor - SCD41, SEN55 (Qwiic)

SEN-25200
$169.95

Get a real-time snapshot of your surrounding environment with the SparkFun Indoor Air Quality Combo Sensor. This board pairs two specialized environmental sensors from Sensirion, the SCD41 and the SEN55, into a single, high-accuracy monitoring station. Instead of chaining multiple separate breakout boards to track different atmospheric variables, this all-in-one board measures CO2, Volatile Organic Compounds (VOCs), Nitrogen Oxides (NOx), particulate matter, temperature, and relative humidity simultaneously!

Was: $184.95 | Now: $169.95


That's it for this week! If you aren't already a subscriber to our New Product Newsletter, you really should be. As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there and be kind to one another! Happy hacking!

15% Off Your First Order on SparkFun Originals!