The ProDriver

Drive stepper motors in a new way with the SparkFun ProDriver! Don't forget to check out the Raspberry Pi HQ Camera as well.

Welcome, all! This Friday, we have something special: The SparkFun ProDriver, a stepper motor driver equipped with the Toshiba TC78H670FTG. That's not all - we also have the new Raspberry Pi HQ Camera Module and lenses to improve the imaging sensing capabilities for your favorite Pi. Let's take a closer look at all of our new products for this first week of September!

All we need is Ryan Gosling to drive a stepper and we'll be good to go!

SparkFun ProDriver - Stepper Motor Driver (TC78H670FTG)

ROB-16836
$22.95

The SparkFun ProDriver makes it easy to start developing with the TC78H670FTG bipolar stepper motor driver from Toshiba. Latch terminals provide instant solder-less connections to every feature offered. Use our extensive Arduino Library with 10 examples, and you can quickly explore the many features of this precise, small-size motor driver IC.


Raspberry Pi HQ Camera Module

SEN-16760
$63.75

The High Quality Camera Module is a camera sensor designed to accept CS-mount lenses and, with the supplied adapter, C-mount lenses for use with the Raspberry Pi single board computer line. It offers higher resolution (12 megapixels, compared to eight megapixels), and sensitivity (approximately 50 percent greater area per pixel, for improved low-light performance) than the existing Camera Module v2. The 12.3 megapixel Sony IMX477 sensor features a 7.9mm diagonal image size and back-illuminated sensor architecture with adjustable back focus. Additionally, this module features an included tripod thread just adjacent to the ribbon cable connector.


Raspberry Pi HQ Camera Lens - 16mm Telephoto

SEN-16761
$125.00

This is the 16mm C-mount telephoto lens for use with the Raspberry Pi HQ Camera Module. The lens produces a 10MP picture in a one-inch image format, and is easily interchangeable using the thumb screw and adapter included with the Pi HQ Camera Module. This telephoto lens excels when taking distance or close-up photos.


Raspberry Pi HQ Camera Lens - 6mm Wide Angle

SEN-16762
$65.00

This is the 6mm CS-mount wide angle lens for use with the Raspberry Pi HQ Camera Module. The lens produces a 3MP picture in a half-inch image format, and is easily interchangeable using the thumb screw and adapter included with the Pi HQ camera module.


Thermal Tape 4x4" Square

PRT-17054
$0.95

Thermally Conductive Adhesive Transfer Tapes are designed to provide a preferential heat-transfer path between heat-generating components and heat sinks or other cooling devices (e.g. fans, heat spreaders, or heat pipes).


That's it for this week! As always, we can't wait to see what you make! Shoot us a tweet @sparkfun, or let us know on Instagram or Facebook. We’d love to see what projects you’ve made!

Never miss a new product!