What is E6 HAS?

A dive into Galileo's free corrections service, which puts the "quad" in "quadband."

Some of our recent products have been described as capable of quadband reception, like the RTK Postcard and LG290P Breakout board. What sets these apart from our other multiband recievers? Like our other high-precision PNT products, they're capable of L1/L2/L5 reception. However, they take it a step further by being able to receive data from the Galileo constellation's E6b band.


The E6 frequency lies between L1 and L2.

In 2018, the European Space Agency began a project called “High Accuracy Service” (HAS). The purpose of this project was to make increased accuracy GNSS available globally by broadcasting corrections directly from each satellite in real-time. Since then, new GNSS receivers have been designed that are capable of receiving and utilizing these corrections, such as the Unicore UM980 and the Quectel LG290P.


Galileo HAS architecture. Source: ESA

Normal GNSS has a peak accuracy of around 1.5 meters, mainly due to the uncertainty of changes to the carrier phase as signals propagate through the ionosphere. In order to get better accuracy than this, the GNSS signals need to be augmented by “corrections”. HAS provides corrections by transmitting them on the E6b band alongside their standard GNSS signals.


So, how does HAS work?

HAS corrections are designed for use in a Precise Point Positioning (PPP) algorithm; a typical use case for PPP would be establishing a very high accuracy position for a Permanent Base Station. Traditional PPP works by having a network of ground stations monitoring satellite broadcasts, computing the error in GNSS satellite broadcasts (and other parameters), and creating corrections for those errors. To compute a corrected position using PPP, a sequential estimation algorithm is used, such as an Extended Kalman Filter, with the goal of finding the following output values:

  • Receiver position (ECEF X, Y, Z)
  • Receiver clock offset
  • Tropospheric zenith delay
  • Carrier-phase ambiguities

There are a number of parameters that need to be corrected for after the ground station network has observed the GNSS signals:

  • Satellite orbit corrections: These refine the broadcast ephemeris data to provide more accurate satellite positions.
  • Satellite clock corrections: These improve the accuracy of satellite clock offset information.
  • Satellite biases: These include code and phase biases for supported Galileo signals.
  • Atmospheric corrections: Not currently available; the full service will include atmospheric (at least ionospheric) corrections, particularly for the European Coverage Area.


Outline of PPP algorithm. It gets a bit complicated. Source

The drawbacks of PPP are the amount of time and infrastructure it requires. The highest quality PPP outcome is only available 12-16 days after the single point data has been collected. The CSRS Rapid PPP has centimeter level accuracy similar to RTK, but is not available until 12 hours after the end of the day the single point data was captured on. For real time, high accuracy operations, RTK is still the best choice.


Source

A unique feature of HAS is that these correction messages are computed for each satellite in the Galileo constellation by a ground station, then uploaded to each respective satellite where they are then broadcast alongside the standard GNSS signals. This allows receivers to run the PPP algorithm in real-time, as long as they are capable of receiving the HAS E6b band, and they have the ability to run the PPP algorithm. In addition to HAS E6-B satellite broadcast, HAS PPP corrections can be obtained through their Internet Data Distribution channel; this distribution channel functions much like NTRIP; you provide credentials, and PPP corrections are piped to your device over the internet using NTRIP.

HAS is an amazing achievement in this way; corrections available nearly worldwide, no base station or NTRIP network required. But, there are some downsides; the accuracy is relatively bad compared to RTK (but still good enough for many use-cases), the process is somewhat slow (5-15 minutes for PPP convergence), and it is sensitive to sudden velocity fluctuations.

What hardware is compatible with Galileo E6b-HAS?

SparkFun sells a few products that are able to receive HAS corrections.

SparkFun RTK Torch

GPS-25662
Retired

SparkFun RTK Postcard

GPS-26916
$219.95

SparkFun Quadband GNSS RTK Breakout - LG290P (Qwiic)

GPS-26620
$189.95

SparkFun Triband GNSS RTK Breakout - UM980

GPS-23286
$459.95

Below is a list of HAS enabled receivers.

Manufacturer Model Segment or Applications HAS channel/s
ANAVS Multi-Sensor RTK/PPP Module Automotive, robotics, maritime, railway, mining and surveying E6b
ANAVS AROX-PPP Autonomous vehicles, Robots, UAVs and Vessels E6b / IDD
Beyond Gravity PODRIX Space navigation, Precise Orbit Determination (POD) E6b
Beyond Gravity NavRIX PinPoint Space navigation, Precise Orbit Determination (POD) E6b
EOS Positioning Arrow Gold+™ Surveying and mapping E6b
Hemisphere Vega Agriculture, construction & mining, machine control, marine E6b
Hemisphere Phantom Agriculture, construction & mining, machine control, marine E6b
Hi-Target iRTK5 Surveying E6b
Hi-Target VRTK Surveying E6b
Kongsberg Seapath® 385 Maritime / hydrographic surveying E6b
Quectel LG290P Surveying E6b
Rokubun SPEAR (SDK) Road navigation, robotics engineering, location-based services, smart agriculture, IoT -
SinoGNSS K803 GNSS OEM module Surveying E6b
South Insight V2 Surveying E6b
South INNO7 (1598) Surveying E6b
South Galaxy G3 Surveying E6b
Spaceopal HAUT HAS validation, surveying, maritime, machine control, aviation E6b / IDD
SparkFun Electronics RTK Torch Surveying and mapping, precise agriculture E6b
Unicore Communications UM980 Surveying and mapping, precise agriculture E6b
Unicore Communications UM981 Surveying and mapping, precise agriculture, intelligent driving E6b
Unicore Communications UM982 UAV and precision agriculture E6b