Let's Get to Rework

Our new Hot-Air Rework Station is here along with a new LED Project Kit, RPi Picos, and Third-Hand Kit!

Hello, everyone! We're back this week with more new products! If you stopped by yesterday, you probably already know about the new Raspberry Pi announcement with the addition of wireless capabilities and headers on two unique Pico boards. On top of that, we have a brand new version of our popular Hot-Air Rework Station with a new set of features that modernizes the instrument for todays standards. Following that, we have have a new LED Project Kit that is ideal for developing minds to start in electronics, as well as a new third hand kit! Alright, let's jump in and take a closer look!

Well... that's a new way to prepare crème brûlée.

Hot-Air Rework Station - 303D

TOL-19101
Retired

This hot-air rework station is great for professionals and hobbyists in need of tight temperature tolerances and large air flows. This unit displays a digital readout of the actual air temperature with a flow rate of up to 23L per minute. This very powerful unit can be used for multiple applications, including standard SMD reflow/repair/removal, thermal IC stress testing, thermoplastic welding, and shrink-wrapping.

This latest version of the hot-air rework station has some great improvement: a new temperature range of 100℃-500℃, an auto sleep function, and a temperature offset function.


Raspberry Pi Pico W

DEV-20173
$6.00 $5.25

The Raspberry Pi Pico W builds upon the great cost-for-performance metrics of the Pico and add WiFi to the board. The Pico W features the same attributes as the Raspberry Pi Pico and also incorporates an Infineon CYW43439 wireless chip. CYW43439 supports IEEE 802.11 b/g/n wireless LAN, and Bluetooth® 5.2. (6/30/2022: Only Wireless LAN is supported on the Pico W at the moment, this will be updated as the new features become available)


Raspberry Pi Pico H

DEV-20172
$5.50

The Raspberry Pi Pico H is a low-cost, high-performance microcontroller board with flexible digital interfaces. It feature the RP2040, which marks Raspberry Pi's first microcontroller designed in-house. Pico provides minimal (yet flexible) external circuitry to support the RP2040 chip (flash, crystal, power supplies and decoupling and USB connector). This variation comes with a set of male headers pre-soldered to all through-hole vias and a 3 pin debug connector. The spacing remains 2.54mm and breadboard compatible (even more so now with the addition of the male headers).


SparkFun LED Project Kit

KIT-19934
Retired

The SparkFun LED Project Kit is a great way to get started with programming and hardware interaction with the Arduino programming language. Each SparkFun LED Project Kit includes everything you need to complete seven projects that will teach you how to blink an LED, create a night light, make a Simon Says game, and more. You don't need any previous programming or electronics experience to use this kit.


Magnetic Third-Hand Kit

TOL-19944
$81.50

If you need an extra pair of hands (or three!) to help with the more delicate, detailed work, you will appreciate this Magnetic Third-Hand Kit. Prefect for any electronic, soldering, crafting, painting, replica, figurine, macro photography and hobby work - or any precision project that requires extreme accuracy.


That's it for this week. As always, we can't wait to see what you make. Shoot us a tweet @sparkfun, or let us know on Instagram, Facebook or LinkedIn. Please be safe out there, be kind to one another, and we'll see you next week with even more new products!

Never miss a new product!